Descargar documento () de 20
We make what matters work*

Módulo de EPRI DRIVE

Mediante la iniciativa de integración de recursos de distribución y estimación de valor (DRIVE), el Electric Power Research Institute, Inc. (EPRI) ha usado muchos años de experiencia en estudios de impactos del sistema detallados y ha desarrollado un método de cálculo simple para ayudar a los servicios públicos de distribución a realizar una evaluación rápida pero precisa de la capacidad de alojamiento de DER del sistema.

El software EPRI DRIVE determina la cantidad máxima de recursos de energía distribuida (Distributed Energy Resources, DER) que cada alimentador de distribución puede gestionar en su estado actual antes de que comiencen a surgir problemas inaceptables térmicos, de confiabilidad, de la calidad de la energía y de la protección.

Integrado de manera transparente en la interfaz gráfica de usuario del software CYME, el módulo EPRI DRIVE se usa como módulo de análisis nativo en el que se combina la sofisticación de la ingeniería de EPRI con las mejoras del modelado del sistema de distribución y las capacidades de análisis de CYME de Eaton.

MÓDULO DE EPRI DRIVE

GENERAL

The calculation method used by the engineer provides aggregate and granular hosting capacity results for each distribution feeder and considers numerous circuit-specific attributes, such as topology, equipment nameplate data, device settings as well as peak and minimum loading conditions. Thanks to its various analysis parameters, it also allows nuancing between different DER technologies, considering the particular impacts of each of the following resource types:

  • Photovoltaic
  • Wind energy conversion systems
  • Battery energy storage systems
  • Fuel cells
  • Microturbines
  • Synchronous generators

Seamlessly integrated into Eaton's CYME software graphical user interface, the EPRI DRIVE module combines the engineering effort of the EPRI DRIVE engine with CYME’s detailed distribution system model to return hosting capacity calculation results within a familiar environment.

FEATURES

The main highlights of EPRI’s hosting capacity method are:

  • Streamlined method based on heuristics
  • Results available for three-phase large DER hosting capacity scenarios (centralized and distributed) and single-phase small DER scenarios (distributed)
  • Thorough analysis based on multiple, diverse criteria covering thermal loading, power quality, protection and reliability
RESULTS

The hosting capacity results are provided under several formats within Eaton's CYME software graphical user interface. Typical for this type of analysis, heat maps and one-line diagram color-coding layers are available for each aspect of the method:

  • Node-level maximum and by-criterion hosting capacity
  • Feeder-level maximum and minimum hosting capacity for each scenario (large centralized and distributed DER, small distributed DER) and criterion

A tooltip is also available on each node of the one-line diagram to consult node-level results (maximum and by-criterion hosting capacity) directly from the distribution system model.

A summary and a spreadsheet report complete the output of the analysis. While the former provides feeder-level results, the latter tabulates the node-level results. Both allow an exhaustive understanding of the distribution system capability to host distributed energy resources.

Funcionalidad

MÓDULO DE EPRI DRIVE

 

 

 

 

 

 

 

GENERAL

El método de cálculo que usan los ingenieros proporciona resultados de capacidad de alojamiento agregado y granular para cada alimentador de distribución y considera numerosos atributos específicos del circuito, como la topología, los datos de la placa de identificación del equipo, la configuración del dispositivo y las condiciones de carga máxima y mínima. Gracias a los diversos parámetros de análisis, se permiten los matices entre diferentes tecnologías de DER, y se tienen en cuenta los impactos particulares de cada uno de los siguientes tipos de recursos:

  • Energía fotovoltaica
  • Sistemas de conversión de energía eólica
  • Sistemas de almacenamiento de energía de la batería
  • Celdas de combustible
  • Microturbinas
  • Generadores sincrónicos

Perfectamente integrado en la interfaz gráfica de usuario del software CYME de Eaton, el módulo EPRI DRIVE combina el esfuerzo de ingeniería del motor EPRI DRIVE con el modelo del sistema de distribución detallado de CYME para obtener resultados de cálculo de la capacidad de alojamiento en un entorno familiar.

CARACTERÍSTICAS

Los aspectos destacados principales del método de capacidad de alojamiento de EPRI son los siguientes:

  • Método simplificado basado en la heurística
  • Resultados disponibles para los escenarios de capacidad de alojamiento de DER trifásicos grandes (centralizados y distribuidos) y escenarios de DER monofásicos pequeños (distribuidos)
  • Análisis exhaustivo basado en criterios múltiples y diversos que cubren carga térmica, calidad de la energía, protección y fiabilidad
RESULTADOS

Los resultados de la capacidad de alojamiento se proporcionan en varios formatos dentro de la interfaz gráfica del usuario del software CYME de Eaton. Lo cual es típico para este tipo de análisis, los mapas de calor y las capas de código de color del diagrama de una sola línea están disponibles para cada aspecto del método:

  • Máximo nivel de nodo y capacidad de alojamiento por criterio
  • Capacidad de alojamiento máxima y mínima del nivel del alimentador para cada escenario (DER grandes centralizados y distribuidos, DER pequeños distribuidos) y criterio

También se encuentra disponible un indicativo de herramienta en cada nodo del diagrama de una línea para consultar los resultados a nivel del nodo (capacidad de alojamiento máxima y por criterio) directamente desde el modelo del sistema de distribución.

Para completar los resultados del análisis, se encuentran disponibles un resumen y una hoja de cálculo. Mientras el primero brinda los resultados a nivel del alimentador, el último permite tabular los resultados a nivel del nodo. Ambos permiten comprender por completo la capacidad del sistema de distribución para alojar recursos de energía distribuida.

¿Necesita soporte para un producto?

Portal de usuarios de CYME: my.cyme.com

Tel.: 450-461-3655 o 800-361-3627 (Canadá & EE. UU.)

Correo electrónico: cymesupport@eaton.com

Preguntas antes de comprar

Correo electrónico: cymeinfo@eaton.com