A reference design provides a convenient foundation for a system-based approach. A reference design defines a preconfigured solution and offers you a blueprint for deployment. Someone with expertise and experience working with OCP standards has validated the engineering design to ensure the components work as a system, removing the guesswork.
There are important power and thermal considerations when selecting a busbar and power shelf combination. All the pitfalls of component incompatibility can be avoided by following a reference design architecture.
A. OCP “OU” mounting rails for 21" (48cm) rack equipment (convertible to EIA rails)
B. EIA “RU” mounting rails for 19" (53cm) rack equipment (convertible to OCP rails)
C. ORV3 busbar (blind-mate power connection)
D. ORV3 power shelf (15 kW N+1; includes six 3 kW modular power supplies)
Note: Shown without doors and side panels.
The Open Compute Project, also known as OCP, was founded by Facebook (now Meta) in 2011 At the time, Facebook were scaling their data centres quickly and dealing with all the challenges that come with that:
Facebook have a strong hacker culture that drives them to find new solutions and shortcuts to move faster. They approached their data centre growing pains with a fresh mindset and proceeded to transform data centre norms, reimagining typical server, rack and power design.
The original OCP rack design was designated Open Rack Version 1 (ORV1). This system was a triplet rack that challenged the traditional EIA 19" (48cm) rack-mount standard, increasing the width to 21" (53cm) and creating a new 1.89" (4.8cm) height standard called “OU” instead of the traditional EIA 1.75" (4.3cm) “RU” height standard. The new approach also introduced a new power topology. In a traditional data centre environment, the servers and networking equipment have individual AC power supplies. The Open Rack standard introduced the power shelf concept. The power shelf is basically a large power supply fitted with modular rectifiers. In the ORV1 standard, the power shelf accepts AC power and distributes 12V DC power to OCP servers using busbars in the back of the rack. This offers several benefits:
In 2016, Microsoft introduced the Project Olympus subgroup of OCP. Project Olympus uses a more traditional 19" (48cm) rack and employs a rack PDU to distribute AC power to the servers.
One unique aspect of the PDU design is the universal input on the PDU, which uses a proprietary connector from Harting. The detachable AC input cord can be configured for different types of power input, allowing one rack PDU to be used at 208V three-phase Delta 60A and 415/240V three-phase Wye 32A. This simplifies deployment by reducing SKU count on rack PDUs and is especially helpful for consistency in global deployments.
Project Olympus was a departure from the power shelf topology, but illustrated that OCP could incorporate a variety of different ideas under its open-source umbrella.
As OCP has grown, changed and included new members and working groups, the focus on improving ORV2 has led to the Open Rack Version 3 (ORV3) standard. ORV3 seeks to address several needs expressed by the OCP community:
OCP is considered by many to be a hyperscale-only platform. It is hard to dispute that companies like Meta, Google and Microsoft drive such economies of scale that they essentially become the platform. That doesn’t mean that smaller business users cannot benefit from OCP standards. Arguably, they can benefit even more by putting to use the lessons learnt from larger-scale deployments.
This still presents challenges, because the OCP model requires a high degree of engineering and direct-to-ODM interaction. It is not common for business customers to have large engineering teams that include mechanical, electrical and power engineers on staff. A data centre manager more often has a small team of network infrastructure experts, software experts and a facility or power engineer. Although a capable team, they typically focus on evaluating commercial solutions rather than designing from scratch. This is where the traditional 19" (48cm) rack and AC power standard has served well for years.
The basic 19" (48cm) rack standard was defined by AT&T around 100 years ago to save space and homogenise installation of telecommunications equipment in telephone company central offices. When telco manufacturers embarked on higher-speed systems, they continued to rely on 19" (48cm) racks. The budding computer industry eventually followed suit and provided AC power supplies for each server.
Today, the 19" (48cm) rack and AC power standard is firmly established and well supported by many different OEM suppliers. Established server vendors such as HPE, Dell, Oracle, Cisco and Lenovo have countless 19" (48cm) server options, refined over many generations. The 19" (48cm) rack standard is supported by companies such as Eaton, APC, Legrand, Vertiv and Rittal, all offering a large selection of racks and related accessories. These racks come in various heights, up to 58U, including the classic 42U, with 24-inch (600mm) or 30-inch (750mm) external cabinet width and various depth options.
Large AC power distribution systems start with a three-phase UPS on the facility side. A typical data centre will have dual-feed power (A and B) throughout the facility, which is distributed to rack enclosures using panel boards, remote power panels (RPP) or overhead busway systems. Inside the rack enclosure, two AC rack PDUs distribute the A and B feed power to redundant AC server power supplies, with two to six power supplies per server.