In case of multiple catalogue numbers, please use comma (",") as the separator.
Please note that the maximum number of catalogue numbers that can be added to one request is 20.
MyEatonFAQs
Enter catalogue numbers below and product specification links will appear on the right.
In case of multiple catalogue numbers, please use comma (",") as the separator.
Please note that the maximum number of catalogue numbers that can be added to one request is 20.
The task can't be completed.
Only Excel97-2016 files (.xlsx) are supported.
The maximum allowed file size is 2MB.
Furthermore, only the first 20 catalogue numbers contained in the file are processed.
Download the example file ->"
Please enter at least one catalogue number
Please add comma and remove the enter space
You cannot request more than 20 technical specifications at the same time.
Enter your email address