Descargar documento () de 20
We make what matters work*

Análisis tecnoeconómico

Las empresas de energía y las instalaciones industriales se enfrentan al desafío de mejorar y desarrollar sistemas eléctricos, mientras garantizan un retorno óptimo de sus inversiones y su viabilidad a largo plazo.
cyme-techno-economic-analysis-product.jpg
El módulo de análisis tecnoeconómico de CYME de Eaton facilita la evaluación de la viabilidad y rentabilidad de un proyecto según un modelo de sistema basado en hechos, lo que conduce a una planificación realista que responde a los objetivos técnicos, financieros y de confiabilidad del servicio. Ya sea que está planificando tareas de mantenimiento, recolocación, mejora o ampliación en un sistema de energía, el módulo tiene como fin ayudar a los servicios públicos y a las grandes empresas a invertir en esa infraestructura analizando los impactos de las modificaciones realizadas, así como el costo y los beneficios que traen aparejados con el paso de los años.  

MÓDULO DE ANÁLISIS TECNOECONÓMICO

GENERAL

For each study, costs can be associated to any modification to the power system model, whether it is the cost resulting from the installation or relocation of an asset or from a load transfer like a phase balancing operation. In addition to the asset cost, economic parameters such as operation and maintenance cost, salvage value and depreciation can be defined and taken into account by the analysis.

The reports creates present load flow results in terms of benefits following reduction in losses and mitigation of abnormal conditions. The economic results include an income statement, a cash flow statement and a capital budget. When used with the CYME Reliability Assessment module, mitigation valuation can be based on improvements of a single reliability index, or a combination of multiple indices.

The Techno-Economic analysis can be performed on a project created using the CYME Advanced Project Manager module. It allows the individual or collective analysis of mitigation projects that are planned for different moments in time. The integration of the two modules brings the analysis to another level by including the technical impacts of concurrent future approved projects, and by allowing a more detailed load growth that combines organic growth, active growth and load transfers.

ECONOMIC FEATURES
  • Economic settings such as the discount rate, the inflation rate and the tax rate are applied on all costs to determine the present value of future cash flows
  • Investment activities (i.e. the costs of the modifications) related to the corrective measures are compared to their economic revenues and gains
  • Analysis can be performed on a calculation period that considers an estimated or forecasted global or detailed load growth
  • Economic results include the Net Present Value (NPV), the Internal Rate of Return (IRR), the Return On Investment (ROI), the estimated payback period and estimated discounted payback period
  • The return on investment is calculated taking into account objectives such as losses reduction, mitigations of abnormal conditions and, an option, the improvement in reliability
  • Asset depreciation over the span of the analysis can be considered along with the possibility to consider the half-year rule and/or to include salvage value and tax
REPORTS

The technical results are available for a base case (i.e. prior to modifications) and for the study/project where the planned measures are applied, for easy comparison.

  • Technical results are presented per-year for the simulation period
  • Technical results used for valuation, i.e. system losses, abnormal conditions and/or reliability indices, are shown with their absolute value and as a reduction compared to the base case
  • Impact of the corrective measures on the power and energy losses (kW and kWh), on the under- and over-voltage conditions, on the overload condition and/or on the selected reliability indices are shown for each year
  • Modifications contained in the study/project for which costs have been defined are also tabulated
  • The economic information shown in the reports include:
    • An income statement (revenues and gains, expenses and losses) for the period simulated
    • A cash flow statement (operating activities, investing activities) for the period simulated
    • A capital budgeting report that gives an overview of the economic indicators such as the NPV, IRR, ROI and the payback period
    • The details of the depreciation calculations related to the figures printed in the income statement are also presented

¿Necesita soporte para un producto?

Portal de usuarios de CYME: my.cyme.com

Tel.: 450-461-3655 o 800-361-3627 (Canadá & EE. UU.)

Correo electrónico: cymesupport@eaton.com

Preguntas antes de comprar

Correo electrónico: cymeinfo@eaton.com