Download document () of 20

New melt-blown polyester depth filter cartridges expand the range of applications offered by Eaton's LOFTOP and LOFTREX M series

NETTERSHEIM, GERMANY … Eaton's LOFTOP™ and LOFTREX M™ depth filter cartridges ensure the safe and efficient filtration of demanding media such as process chemicals, fine chemicals, acids, alkalis and solvents, as well as paints, lacquers and resins. The Filtration Division of the energy management company Eaton is now expanding its range to include filter cartridges that use polyester as the filter material for particularly high chemical resistance. The new melt-blown polyester depth filter cartridges are not only suitable for a variety of aggressive media, but also provide an alternative to filter cartridges that are bonded with phenolic resin. The entire LOFTOP and LOFTREX M filter cartridge range is now available with polypropylene (PP), polyamide 6.6 (PA) or polyester (PES) filter material.

The filter cartridges are available in different lengths and with all common adapter configurations and sealing materials so that they can be used safely in a wide range of applications and filter housings. LOFTOP depth filter cartridges offer absolute retention rates from 0.50 to 120 μm with a retention efficiency of 99.98%. LOFTREX M depth filter cartridges offer nominal retention rates from 1 to 150 μm with a retention efficiency of 95%.

Demanding applications require suitable filter media

When choosing a suitable filtration system, the chemical resistance of filter materials is one of the most important factors for users in many industries, particularly the chemical production industry. In this industry, many processes involve filtering demanding or aggressive media that would damage unsuitable filter materials. "In the chemical industry, everything interacts with everything else," says Alexander Bachmann, describing the challenge. The senior application engineer of Eaton's Filtration Division states: "For media such as paints and solvents, it is necessary to ensure both chemical and thermal resistance—even in the case of aggressive properties." For various media, these requirements can be fulfilled by filter cartridges that use polyester as the filter material.

"By expanding our filter cartridge range, we can provide users with additional and, above all, reliable options for their filtration processes," continues Bachmann. For example, manufacturers and producers of paint resins have so far relied on filter cartridges bonded with phenolic resin for filtration. Although these filter cartridges offer the necessary chemical resistance, their manufacturing process and disposal means that they are becoming increasingly incompatible with stricter environmental requirements. "Melt-blown polyester filter cartridges provide users with an alternative to filter cartridges that are bonded with phenolic resin," says Bachmann.

Reliable filter materials for all requirements

No matter whether the filter material consists of PP, PA or PES, Eaton's LOFTOP and LOFTREX M depth filter cartridges offer a solution to the many challenges of filtering media safely and reliably in the chemical and other industries. They are made of high-purity microfibers, which are blown in a controlled manner onto an inner core and thermally bonded in the same process step without the use of additives. The filter cartridges do not contain any adhesives or binders. They are individually sealed in foil to reliably prevent cross-contamination prior to installation, and offer a high dirt-holding capacity in a wide range of applications.

About Eaton’s Filtration Division:

Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit Eaton.com/filtration.

Eaton is an intelligent power management company dedicated to improving the quality of life and protecting the environment for people everywhere. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we’re accelerating the planet’s transition to renewable energy, helping to solve the world’s most urgent power management challenges, and doing what’s best for our stakeholders and all of society.

Founded in 1911, Eaton is marking its 100th anniversary of being listed on the New York Stock Exchange. We reported revenues of $20.8 billion in 2022 and serve customers in more than 170 countries. For more information, visit www.eaton.com. Follow us on Twitter and LinkedIn.

Contact
Uta Hilgers
+49 6704 204 204
LOFTOP
High chemical resistance and a wide range of applications: New LOFTOP and LOFTREX M melt-blown polyester depth filter cartridges in various designs enable users from different industries to safely and efficiently filter demanding media.