The new version of IPM has the same IT server and cluster shutdowns as the old version but with a new and greatly improved user interface and LDAP/Active Directory compatibility. With the new platform, users can now monitor and manage more nodes.
Even though the function is the same as IPM 1, the IPM 2 interface has changed along with the functionality of setting new automation policies. In addition, IPM 2 is on an entirely new platform. IPM 2 cannot be upgraded from IPM 1. It requires a new separate installation because of the new platform.
Learn more about differences between our Intelligent Power Manager versions.
Any NUT (Network UPS Tools) supported UPS will communicate with IPM 2. IPM 2 treats them the same as a premium Eaton UPS and the user gets whatever functions are available in the IPM edition they are using:
If you are not seeing any data from a rack PDU, please check: