Research shows marked improvement in both the ability to access skilled staff and openness to move away from legacy technology in order to accelerate digital transformation efforts.
In 2022, 29% of organizations said skills and staff shortages were holding them back vs. 23% today. We also saw a significant improvement related to reliance on legacy technology. In our last survey 33% of respondents said that legacy technology was holding them back. Now, just 23% have similar views, signalling willingness to take advantage of new digital tools like AI.
There’s a big gap between expected technology application and actual deployment
Half of enterprises today are executing their digital transformation strategy, with most others in the consideration phase. But less than a quarter of survey respondants have broadly adopted digital technologies to assist them in the transformation efforts. When it comes to AI/ML technologies, predictive analytics – which can impact operations most directly – is the most in use or planned flavor in use by OT-powered organizations today.
The technologies and tools to implement digital transformation are evolving and expanding quickly as well. Cloud and cybersecurity deployment grew the most over the past two years, cementing those two critical technologies as lynchpins of digital transformation. Cloud changes the economic and operational underpinnings of information technologies. Cybersecurity sits at the crossroads of digital opportunity and risk, assuring that even as enterprises open up digitally, they protect themselves from theft and disruption.
AI/ML Predictive is most in-use, in deployment or planned use by 29% of respondents. The manufacturing sector, which has deployed machine learning to automate assembly lines and improve maintenance programs, was on top with 43% of respondents deploying the technology
Generative AI is in deployment or planned by 26% of respondents, deployed in relatively equal measures across the four sectors surveyed. Generative AI is helpful in its own right, but has the potential to be an even bigger change-agent when coupled with AI/ML, building agents that can act on their own with intelligence and autonomy
Finally, computer vision is planned or deployed by 21% of respondents, again largely equally across sectors. It is perhaps most pertinent in manufacturing, where computer vision can help in sorting or quality control operations but has a place in other industries as well.