下載文件 () / 20

Adding digital performance to MCCB

Predictable and safer operation with digital Moulded Case Circuit Breakers (MCCB)

On top of the overload protection MCCB with digital trip units can even increase the availability of production lines and the security of the personnell working with it. Thanks to the lifecycle management predictive maintenance becomes an easy exercise. The integrated arc flash protection improves safety during maintenance and the integrated metering can be used for condition monitoring and energy management systems.
eaton-bottling-machine

The tripping of a circuit breaker due to an overcurrent is important as it protects machines and other assets from damage. On the other side such a trip of a circuit breaker usually leads to a production interruption. Once the root cause for incident is eliminated operations should re-start as soon as possible. But is the breaker still in good conditions to go into live operation again? Or does it have to be exchanged to avoid malfunction and even bigger outages with the next overload current or short circuit? Read our whitepaper about how the lifecycle management function in the new digital MCCB trip unit can help you run your business safely at all time.

In high profile production sites or operations with critical processes every interruption can become extremely costly. Therefore maintenance may have to be done under live voltage. Digital MCCB from Eaton provide simple to use arc flash reduction systems that are designed exactly for such maintenance services. While working on the cabinet or machine the system provides a safer working envirionment and the system can be automatically reset to normal operation when cabinet doors are closed. Thus production lines can run without interruption while the maintenance teams always benefit from maximum safety. 

 

Technicians doing maintenance on a panel board
Analog energy metering device

The fact that the exploitation of resources can not be continued in its current form is becoming the central political issue in more and more regions of the world. The pressure on governments and the industry to implement sustainable measures to reduce energy consumption is steadily increasing. Many governments have already implemented programs to support companies that are implementing energy-saving measures. In Europe the access to such benefits is very often tied to the introduction of an energy management system according to ISO 50001. What needs to be considered when it is planned to introduce an energy management system we have summarized on the following page.

Smart factory using digital main switch for their energy management system

If smart factories want to reduce their energy consumption continuously, the introduction of an energy management system according to ISO 50001 is the first important step. But only if the measurement accuracy of the components used is sufficient and the collection of data is really consistent, sustainable results can be achieved.
eaton-schrems-austria-man-looking on-display

The smart factory of Eaton in Schrems produces several thousands of electrical switchgear each year. Their annual consumption of Energy is as high as 111 MWh. Installing an energy management system according to ISO 50001 helps them to safe more than xx% of energy each year. Thanks to the new digital MCCB NZM the capturing of data with the machines and the communication to the central Manufacturing Execution System (MES) has become much easier than in the past.

Make your operations safer, more predictable and more energy efficient with the digital moulded case circuit breakers (MCCB) NZM

Thanks to the big variaty of available field bus communication and the comprehensive program of accessories the digital moulded case circuit breaker NZM can be easily integrated into machines and power distribution systems in smart factories. It can be perfectly combined with the other Eaton circuit protection and motor control devices to build reliably operating machines and systems. The highly accurate metering capabilities of the breaker make it the ideal device to provide energy data into energy management systems that fulfill the requirements of ISO 50001.

Featured products & services

xSpider design tool for low-voltage networks

The xSpider software system is a graphically oriented design system for dimensioning of low-voltage networks fitted with Eaton brand circuit protection equipment. It calculates voltage drops, load distributions and short-circuit currents for radial as well as meshed networks and carries out a subsequent check on the suitability of the cables and protection equipment used. The software is intended primarily for designers and computational engineers.
540567758
Digital NZM Molded Case Circuit Breaker
Digital residual current circuit breaker FRC
Digital residual current circuit breaker
Digital residual current circuit breaker , SmartWire-DT
Digital residual current circuit breaker with SmartWire-DT connection
PXS24 Protection Module
PXS24 protection device for 24 VDC circuits
eaton-motorstarter-pkz-pke
Motor starter combinations