Download document () of 20
We make what matters work*

Protective device coordination (CYMTCC)

Engineers are often called upon to visualize the protection of their networks quickly and easily.
Eaton's CYMTCC software addresses time over-current protection for industrial, commercial and distribution power systems. The program comes with an extensive database of over 15,000 protective devices from more than 100 different manufacturers that are easily accessed to produce time-current curve plots and device settings reports. It also features several tools and reports to help you achieve coordination and protect transformers and cables. Eaton's CYME arc flash hazards analysis module can be added to the CYMTCC software to further complement the analyses.

Protective device coordination software

Features

Eaton's CYMTCC software provides a powerful editor that allows building the network one-line diagram by simply clicking and dragging device symbols onto the drawing. The time-current characteristic curves for the protective devices can be visualized onscreen, plotted on standard log-log paper and routed to various printers. The one-line diagram and the time-current curve can be exported to files for inclusion in other reports as well.

The program is capable of generating all the necessary study benchmarks such as cable and conductor damage curves, motor starting curves, transformer withstand curves, inrush and thermal points and offers comprehensive graphical and tabular means for verifying the curve clearances at any fault current or system voltage level.

Analytical capabilities

  • Curve dragging option to adjust coordination
  • High-quality graphic display and output
  • Printing on log-log paper (curves only) or on plain paper (curves and grid)
  • Accounts for LL and LG through-faults on delta-y transformers
  • Coordination and protection verification based on user-defined criteria
  • Interactive analysis reports
  • Powerful tools to measure separation time between each pair of devices
  • Electronic reclosers from several manufacturers such as Eaton, Schweitzer, S&C , ABB and more
  • Control of current scale, colors, curve hatching, ID tag location, title block style and more
  • Facility to import external graphic file (e.g., a company logo) to the curve plot or to the one-line diagram
  • Facility to export the curve plot to PDF, JPG, AutoCAD DWG/DXF, SVG (XML), and other formats
  • Ability to open two or more studies; copy curves from one to another and make modifications rapidly to all the opened studies
  • Automatic relay time dial selection based on desired operating time
  • Ability to enter numerical equations to any type of devices
  • Enhanced search tool to find and create devices rapidly and it is also possible to create a list of favorite devices

Device library

Eaton's CYMTCC software includes an integrated device library manager program that allows the user to add new device characteristics to the database and to modify existing curves. Note that our team can also add curves for you if you provide the data.

The devices are categorized and stored by manufacturer name and device type for easy retrieval. The database contains more than 15,000 devices from North American, European and Asian manufacturers.

It features low-voltage circuit breakers (electromechanical, solid state and molded case), fuses, relays (electromechanical and electronic) and reclosers (hydraulic and electronic).

The device library is updated regularly and you may update your own library using the “online update” directly from the software (if you have an internet connection). 

Need product support?

CYME users portal: my.cyme.com