NEW! Launched in June 2021.
Includes all versions before June 2021 and on-going support through to 2023.
The new version of IPM has the same IT server and cluster shutdowns as the old version but with a new and greatly improved user interface, LDAP/Active Directory compatibility. With the new platform, users can now monitor and manage more nodes.
Even though the function is the same as IPM 1, the IPM 2 interface has changed, as has its functionality of setting new automation policies. In addition, IPM 2 is on an entirely new platform. IPM 2 cannot be upgraded from IPM 1. It requires a new separate installation because of the new platform.
For a 60 day free trial of the IPM Optimise licence with advanced capabilities, please complete this form.
To upgrade an existing IPM licence, please see below.
Any network-connected UPS, compatible with NUT (network UPS tools) acquisition engine will communicate with IPM 2. IPM 2 treats them the same as a premium Eaton UPS, and the user gets whatever functions are available in the IPM edition they are using:
If you are not seeing any data from a rack PDU, please check:
Yes, Eaton offers a full range of installation services. For IPM, we offer both one-day and two-day installation service based on the size of the user’s environment.
For specific part numbers on these IPM installation services, see the table below:
On-site service offerings |
Part number |
| IPM installation on-site: one day service | SW06NXXX-001X |
| IPM installation on-site: two-day service | SW05Nxxx-002X |