Lae dokument alla () … 20
We make what matters work*

WaveStream LED takes design flexibility to an entirely new plane.

WaveStream LED

LED technology has long been hailed as the future of lighting technology. Despite the energy savings, lower maintenance costs and impressive lifespan, something has been holding the LED revolution back. And it might just be pure aesthetics. Especially in architectural environments, the “pixelated” appearance and glare of LEDs have overshadowed any cost benefit.

This got Eaton thinking: What if we could reimagine the way LEDs worked, right from the source, and take lighting design — and the industry — in an entirely new direction?

New reflections on what a reflector can be

The fundamental job of a lighting fixture is to steer light as it leaves its source, typically using reflectors, diffusers or other mechanics. But when you consider LED applications in backlit and edgelit electronics displays, it opens the door to some radically different thinking.

The breakthrough came when engineers realized they could make a light panel act like a reflector, effectively combining two components into one. By molding complex patterns of tiny, computer-designed “prisms” into optical-grade acrylic, it became possible to redirect edgelit LED light with exceedingly high precision and accuracy. And WaveStream was born.

patented_optics.jpg
The science behind the beauty.
Patented optical coupling maximizes the amount of light injected into the WaveStream panel, dramatically improving luminaire efficiency. Laser-precise AccuAim optics arranged in exacting patterns provide unparalleled brightness control while delivering optimal distributions tailored to each fixture and application.
While being incredibly efficient (85%—95% of the light that goes in comes out), what’s really getting noticed are the innovative design possibilities. WaveStream can be molded into virtually any edgelit shape — squares, circles, rectangles and cylinders — to meet exacting specifications and achieve precise lighting results. And because there is no need for a reflector the overall profile of the luminaire is not simply decreased, it can be completely rethought.
Note - Explore our products - In this section we can add only 9 products. If I am adding 1 more product to this then it won't show anything.

Energizing your business.

When companies have to constantly do more while using less, Eaton’s B-Line series 4Dimension strut system is revolutionizing the way installers build and install critical infrastructure support systems. From electrical and mechanical, to HVAC and plumbing applications, to the most advanced data centers, Eaton is bringing the world a whole new dimension of form, function and flexibility.

Learn about the Eaton’s B-Line series 4Dimension strut system, explore Eaton structural support solutions and see how Eaton innovation is energizing customers’ businessacross industries and around the world.

Video: Eaton's B-Line series 4Dimension changes how support systems are built and installed.
  • Data center industry insights

    Learn more about how you can optimize your data center by exploring our knowledge center
    Explore more