문서 다운로드 () / 20
당신의 필요한 일, 이튼이 합니다*

Coolant distribution units and liquid infrastructure for data centers 

Why CDUs anchor liquid cooling systems

As liquid cooling adoption grows, the coolant distribution unit (CDU) becomes a foundational element of the thermal architecture. It establishes stable operating conditions between IT hardware and facility systems, shaping how reliably liquid cooling can be deployed and expanded. Early decisions around CDU capabilities often determine whether liquid cooling remains manageable as density and complexity increase.

Efficiency metrics and regulatory pressure

Liquid infrastructure decisions increasingly intersect with regional efficiency goals and reporting requirements. CDU design and control strategy can influence performance metrics such as European Power Usage Effectiveness, making cooling infrastructure a visible contributor to overall energy efficiency outcomes rather than a hidden backend system.

Supporting advanced computational demands

AI workloads place sustained and variable demands on cooling systems that traditional approaches struggle to absorb. Liquid infrastructure designed to maximize AI cooling focuses on maintaining consistent temperatures under changing load profiles. CDUs play a central role by regulating flow and thermal response as power levels fluctuate at the rack level.

Integrating liquid cooling at scale

Successful CDU liquid cooling deployments depend on how well pumping, heat exchange and controls are matched to real operating conditions. Mismatched capacity or poorly tuned controls can introduce instability that offsets the benefits of liquid heat transfer. Infrastructure alignment is therefore critical as cooling strategies move from pilots to production environments.

Positioning CDUs within the data center

How a data center CDU is positioned within the facility affects scalability, service access and long term flexibility. Infrastructure placement decisions influence distribution complexity and determine how easily additional racks or rows can be integrated without a redesign. Thoughtful placement helps reduce friction as cooling requirements evolve.

Rack level infrastructure considerations

As liquid is delivered closer to the IT load, configurations such as the in rack CDU introduce new design and service tradeoffs. These choices influence distribution length, accessibility and risk containment. Understanding these implications early supports smoother expansion and more predictable operational behavior.

Liquid infrastructure for scalable data center cooling

Liquid infrastructure is central to enabling scalable, reliable liquid cooling in modern data centers. Coolant distribution units influence thermal stability, efficiency and operational consistency as workloads grow denser and more dynamic. By understanding how CDU design, placement and control affect system behavior, organizations can deploy liquid cooling with greater confidence and long term performance predictability.