Positive Temperature Coefficient (PTC) devices are simple, inexpensive, but critical circuit components that protect against overload or short-circuit (fault) conditions. Although multiple differences exist between PTCs and traditional one-time fuses, the most notable is that PTCs can allow current to flow after the fault is cleared without replacing the device, often referred to as resettable.
This technical note introduces the basic concepts of the PolyTron™ PTC devices, their main features, benefits and typical applications. A detailed description of their operation, fault and protection modes, and typical circuit diagram is explored. Specific product details and ordering information is available on the data sheets at www.eaton.com/elx-datasheets.
Note the terms below are related to DC operating parameters:
PTC devices exhibit a positive temperature coefficient (resistance increases exponentially with increased temperature) allowing them to protect circuits exposed to increased currents or temperature. The PTC device protects itself and the circuit by increasing its internal resistance in the event of a short-circuit or overcurrent event as depicted in Figure 1.
Figure 1 also shows the counterpart to the PTC, a negative temperature coefficient (NTC), which is a device where the internal resistance decreases as the temperature increases. This feature makes NTCs useful in applications such as push-pull amplifiers, battery protection and sensor applications.
Figure 1.
Positive and negative temperature coefficient curves
Figure 2.
Conductive paths for normal and tripped states
Figure 3.
Typical PTC application: Single/multiple supply line protection
The following is a short summary of the general differences between PTC devices and one-Time fuses.
Leakage current:
Fault current:
Operating voltage rating:
Hold current rating:
Temperature derating:
Resistance:
Time current characteristics:
Key parameters are important to help detrmine which PTC device is best suited for an application. The following is list of basic questions and guidlines that will aid in the selection process.
1. What is the normal operating current (Ihold) expected in the circuit?
2. What is the maximum circuit voltage (Vmax)?
3. What is the maximum fault current (Imax) in the circuit?
4. How fast does the PTC response need to be?
5. What is the maximum power dissipation during the tripped state?
6. What is the resistance ratio (normal vs. tripped)?
7. Verify the installation layout for proper selection product type.
The following information provides in-depth details of some of the key parameters and data sheet specifications.
The Eaton PTC data sheet provides a table of key specifications needed for selction of a device. Figure 4 provides a snap-shot speciifcation table data sheet example. Selecting the PTR016V0090 as the example, it can be detrmined that the maximum voltage allowed is 16 Vdc and the maximum current allowed is 40 A. The hold current is 0.9 A and the trip current is 1.8 A. This device has a 0.6 W maximum power dissipation and takes 1.2 seconds to trip at 8 A maximum. The initial resistance is 0.07 Ω that increases to 0.18 Ω in tripped mode.
Figure 4.
Data sheet specification table
Figure 5.
Typical time-to-trip curve
The time-to-trip curves are a usefull tool to help detrmine the proper needed trip current for an application. Each PTC value has a colored line representing the time it takes to trip for differnt current values.
Using the example curve in Figure 5 and following the yellow line from the top of the graph to the bottom, the PTC device represents typical trips at:
Temperature directly affects the performance of the PTC device. Derating of the specified or rated current is necessary to accommodate operating temeperatiures above or below the rated current specifications. The thermal derating curve is the tool to be used to help determine the proper derating.
Figure 6 is a typical derating curve example. One can select the temperature (horizontal axis) with the derating point (vertical axis). For example, the 100% derating point intersects the line at +20 °C.
To better understand this graph and the PTC behavior, the following are examples using the derating curve.
The example parameters are +20 °C and 100% derating corresponds to a current Ihold of 1 A.
If the PTC device is operating at -20 °C, the % derating is 130%.
The new current rating would be I(-20 °C) = Ihold * 1.3 = 1.3 A
If the PTC device operates at +80 °C, the derating % would be 50%. The new current would be I(+80 °C)= Ihold * 0.5 = 0.5 A
In summary, the PTC hold current (Ihold) is:
Increasing the operating temperature above +20 °C, the hold (or trip) current is reduced by a factor of 0.5 (50%). The opposite is true for low temperatures. By decreasing the operating temperature (below +20 °C) to -20 °C, the hold (or trip) current is increased by a factor of 1.3 (130%).
The designer must be aware of the variation of the circuit’s operating temperature and apply the correct derating to ensure proper circuit protection operation.
Figure 6.
Typical thermal derating curve
Figure 7.
Trip time vs trip current temperature dependency
Trip time vs. current, measured at different operating temperatures (0 °C, +20 °C and +60 °C) illustrates the the temperature influence on the trip time and current depcted in Figure 7.
For a 5 A trip current the trip/response time is about 1 second @ +60 °C, 10 seconds @ +20 °C and 10,000 seconds @ 0 °C.
The higher the temperature, the shorter the trip time. The designer should understand the variation in trip time with temperature and consider how the trip time affects the specific application.
PTCs are available in a variety of sizes, shapes and packages both surface mount and through-hole making them suitable for a wide range of circuit protection applications. Figure 8 displays a snapshot of the Eaton PTC product offering.
Eaton offers a complete range of overcurrent and overvoltage protection solutions, including the PTC, one time fuses, and ESD suppressors. These solutions are suited to fit even the most complex application requirements in terms of currents, voltages, response
Figure 8.
Eaton SMD and through-hole PTC product offering
Figure 9.
Typical PTC and ESD USB 3.0 application.
For more complete circuit protection against ESD faults and shortcircuit, PTCs are typically complemented by ESD suppressors, providing full circuit protection (current and voltage).
The USB example in figure 9 shows the PTC device protecting the circuit against short-circuit or overload on the USB supply line. The ESD suppressors protect the data lines against any voltage spikes that can damage the microcontroller or the load.
Figure 10.
Rechargeable battery pack
Figure 11.
Notebook/laptop protection for I/O Ports, USB and A/V.
Figure 12.
Motor drive protection
Figure 13.
Telecommunication equipment