Download document () of 20

AI approach improves fire prevention

Annually in the EU, approximately 1.8 million fires occur in homes and commercial buildings.  Shockingly, 25% of these fires are ignited due to an electrical failure.  The center for intelligent power (CIP) played a pivotal role in enhancing Eaton’s line arc fault detection devices (AFDDs) through a structured approach to data analytics and the application of machine learning.

Arc faults, which are electrical anomalies, can lead to fire hazards if not detected and mitigated promptly. While AFDDs are excellent tools to mitigate arc faults, they are only as good as our ability to trust their accuracy. 

 

When it comes to arc faults, even occasional false alarms can lead to complacency.  Installers and homeowners need a reliable way to ensure electrical safety and prevent unnecessary tripping, which can be disruptive and costly. 

Eaton's center for intelligent power (CIP) was challenged by our product team to improve the accuracy of its legacy AFDDs. The requirement was to engineer an accurate arc fault detection system that can not only discern genuine arc fault events from non-threatening anomalies but also one that could improve over time based on accumulated data analytics.

Here's how we are approaching the challenge:

First, the data science team collected extensive data from various AFDDs in operation, which included information on normal electrical patterns as well as anomalies that led to arc faults.

By investigating the collected data, the team has been able to identify common characteristics and signatures of arc faults. They are currently developing machine learning models that are capable of distinguishing between actual arc faults and other electrical events. These models are being 'trained' using the collected dataset to ensure high sensitivity and specificity.

The machine learning algorithms are being continuously optimized through iterative testing and validation. The research team is employing advanced analytics to improve the detection algorithms, in order to reduce the risk of incidence of false positives and negatives.

Furthermore, to validate the accuracy of the AFDDs, extensive real-world testing is being conducted. Feedback from these tests will be used to further enhance the algorithm, ensuring its reliability and trustworthiness in diverse electrical environments.

Recognizing the dynamic and complex nature of electrical installations and usage patterns, the research team is also developing a feedback system designed to ensure ongoing improvement. The AI models are designed to learn from new data, adapting and improving over time to maintain high accuracy levels.

Here are some benefits of using Eaton's AFDDs enhanced by machine learning:

  • Enhanced Sensitivity: Eaton's latest algorithms offer improved sensitivity to various types of arc faults, including both parallel (line-to-line) and series (line-to-load) arcs. This can provide a more accurate detection of actual arc faults while minimizing false trips.
  • Adaptive Learning: Eaton AFDDs incorporate advanced algorithms capable of adapting to different environments and electrical loads. This means the AFDD could learn the electrical 'signature' of your home or facility, reducing the chances of nuisance tripping that can be common with less sophisticated devices.
  • Wide Detection Range: Eaton's AFDDs will be equipped with algorithms that can detect arcs over a wider range of currents and frequencies, which enhances their ability to protect against a greater variety of potential electrical fire scenarios.
  • Selective Tripping: Using a smarter live algorithm, Eaton AFDDs can more accurately discriminate between fault conditions and normal operating conditions, leading to selective tripping only in actual fault scenarios. This ensures essential circuits remain powered unless a real threat is detected.
  • Reduced Nuisance Tripping: Advanced algorithms can reduce nuisance tripping, a common issue with early arc fault detectors that react to normal Operating conditions like switching on and off appliances. This increases reliability and user confidence in the system.