In the aftermath of recent natural disasters, and the increasing cyber threats, many states are beginning to offer grants to install infrastructure to address the need for power reliability and grid resiliency. Further, in other parts of the world, over one billion people still lack access to electricity. Microgrids provide an excellent platform to keep the power on and operate critical assets over long periods of time, isolated from a damaged grid as well as to bring electricity to developing parts of the world. But what configuration and components are optimal for your specific power needs? Do you need prime generation or standby distributed generation assets and what types? What is the most economical way to power your microgrid while keeping it resilient?
Feasibility study: The process
The technology is available today to allow microgrids to function with both prime or standby distributed generation assets during times when the grid is healthy and operating properly, while also having the capability to physically disconnect from the grid and operate in an islanding mode for extended periods of time powering critical infrastructure. Each circumstance and set of requirements is unique and must be considered carefully when developing the strategy and execution plan to provide energy reliability. For that reason, it is important that a careful analysis of risks and needs specific to each situation is fully reviewed and understood.
From that analysis, a comprehensive and tailored energy reliability plan can be developed. Specific contingencies should be examined and addressed in the resulting action plan. Eaton works with you to identify each critical asset (facilities and applications) addressed in the study in terms of energy needs and the criticality of each identified asset. Based on your identified power-critical assets, load sizes and profiles, location of supply and storage infrastructure necessary to adequately support critical assets will be identified and designed into the proposed system. Renewable energy assets, if desired, can also be incorporated into the microgrid design. Additionally, the type and availability of the fuel to power other distributed generation assets is evaluated under the foreseeable contingencies and environmental rules.
Feasibility study: Aspects
Our team of experienced engineers will provide a costeffective feasibility study for building a system to maximize uptime and reliability, while also addressing financial factors. Our approach investigates and provides all or some of the following:
Feasibility study: Potential recommendations
Recommendations from Eaton’s microgrid study and consultation could include:
Why choose Eaton?
Eaton’s Electrical Engineering Services & Systems team is one of the largest and dispersed group of experienced engineers and technicians. We offer extensive experience in electrical power distribution systems design, feasibility studies, installation, startup, commissioning, maintenance, troubleshooting, life-extension and ongoing monitoring of operating parameters as well as failure indicators.
For more information or if you have any questions or requests, please visit Eaton.com/service or Eaton.com/microgrid to find your local Eaton engineering services.