In addition, an arc flash study should include a discussion of the operating scenarios considered, including normal utility operation and alternative sources of power such as diesel standby generators. Incident energy numbers calculated in the arc flash study also determine what kind of personal protective equipment (PPE) is required.
For employee safety, OSHA requires that this information be based on the most current version of NFPA 70E, documented, and up to date.
In the past, the industry focused on arc flash mitigation at areas that had “high” incident energy or in other words, where standard PPE would not be enough to protect a worker from an arc flash.
Now, NFPA 70®, National Electric Code® (NEC) has a prescriptive approach to reducing incident energy.
The scope of the NEC Arc Energy Reduction requirements applies to all fusible (Section 240.67) and circuit breaker (Section 240.87) devices 1200 A and above.
For fusible devices, the fuse must have a clearing time of 0.07 seconds or less at the available arcing current, or one of the below approved methods for arc energy reduction must be implemented:
For circuit breaker devices, there are seven approved methods for arc energy reduction that facilities may employ:
In addition, both sections require:
While the NEC provides a number of options, it is important to know that not all solutions are equally effective. Certain methods approved by the code might not be the right solution for every application. Exploring all options and understanding the advantages and limitations of each will help determine the best possible plan for a facility.
Eaton’s arc flash experts are trained to assess every factor contributing to a facility’s arc flash risks and recommend the right solution to maximize safety. Additionally, Eaton offers a wide array of products and services to help you achieve arc energy reduction and compliance with NEC 240.67 and NEC 240.87.
Before making a purchase plan, contact a power systems engineer to confirm the arc energy reduction solution selected will achieve the expected incident energy reduction level.
Once your arc flash solution has been implemented, it is important to update the arc flash labels to reflect the reduced incident energy levels. Typically, per NFPA 70E, labels are required on equipment that is likely to need service or maintenance while energized, such as:
These labels require specific information be prominently displayed:
While not required, adding the date the available fault current was calculated on the label will be an indicator to update the calculation if changes are made to the system.
Need help determining the best mitigation plan for your facility? Eaton can help.
Download