Download document () of 20
  • SMP 16 gateway automation platform upgrade program

    Eaton is offering special incentives to help our customers transition to the latest SMP SG-4260 automation platform.

Upgrade now

Complete this form to take advantage of these special incentives and upgrade to the SMP SG-4260 automation platform.

The last software version supported on an SMP 16 automation platform is version 8.0; the support for this version ended as of April 2023 and the hardware support ended as of June 2025.

To help make the conversion to the latest platform easier, Eaton is offering free software license tranfer from SMP 16 to SMP SG-4260 automation platform as a special upgrade incentive for current users of the SMP 16 automation platform.

Upgrade now to the latest SMP SG-4260 automation platform.

automation-platforms-smpsg-4260-dualps.jpg
For details about the end of support of the SMP 16 automation platform, refer to the SMP Gateway Life Cycle and compatibilities table on our client site. You must create an account to access the site; contact PSMO-Sales@Eaton.com if you are experiencing difficulties accessing the site or creating an account. 

Key reasons to upgrade now to the SG-4260 platform

  • Seamless transition of configuration and tools
  • Optional dual power supply for uninterrupted operation
  • Optional Advanced Ethernet Module (AEM)
    • 4 ports 100/1000BASE-T or 4 ports 100BASE-FX (LC or ST connectors)
    • Implements Standard/PRP/HSR Ethernet protocols for higher system availability (redundant networks). Also implements time synchronization via PTP protocol — IEEE Std 1588-2008
  • Flexible Ethernet connectivity with two (2) built-in SFP ports (option, 1GbE)
  • Optional satellite-based time synchronization (GNSS) for the GPS and GLONASS constellations
  • Support of new software and tools updates on the automation platform
  • Extended input voltage range on the SMP SG-4260
  • Optional satellite-based time synchronization (GNSS) for the GPS and GLONASS constellations (only GPS is available on the SMP 16)
  • Smaller form factor (2U instead of 3U) for less rack space
  • Console port is USB type on the SMP SG-4260 (accessible through Ethernet connection for maintenance and configuration) instead of the serial port on the SMP 16
  • Optional additional storage option on an SSD drive (field upgradable) instead of flash drive
  • Greater video resolution on HMI local screen
 

Upgrade now

Complete this form to take advantage of these special incentives and upgrade to the SMP SG-4260 gateway automation platform.

By submitting this form, I agree that the personal data that I provide can be shared with Eaton, channel partners and third-party providers working on behalf of Eaton in accordance with the Eaton Privacy Policy and in compliance with applicable data privacy laws.

I agree to be informed regularly about Eaton products, promotions and news. I understand and agree that Eaton will use my data to personalize marketing communications.  I agree that the personal data that I provide can be shared with Eaton Corporation plc in Ireland, Eaton Corporation in the United States of America and for storage in electronic marketing databases hosted in Canada. Any use of my personal data will take place in compliance with the relevant and applicable data privacy laws and the Eaton Privacy Policy. I can withdraw my consent to receive marketing communications at any time by contacting Eaton.

About Eaton’s SMP gateway automation platform

automation-platform-smpsg4250.jpg
Eaton's SMP gateway automation platform combines all the functions required by modern automation systems including innovative functionality, high reliability and scalability in a single powerful package. In addition to providing data concentrator, protocol translator and logic processor functions, the SMP gateway features an integrated HMI and facilitates secure remote access for maintenance to substation and field devices, reducing operating costs and increasing productivity.