Download document () of 20

IT Gaming solutions for your every need

 

 

 

Empowering gamers with solutions for uninterrupted performance

Imagine you're on the brink of a new personal best or locked in a crucial online match. The thrill of the game is at its peak, and then... an unexpected power outage pulls the plug on your victory.

But what if you could protect your game from such interruptions? With Eaton's IT Gaming Solutions, you can! Power, protect and connect your gaming setup and turn the tables on power outages.

Don't just play the game, conquer it. With Eaton, you're always in control. SAVE YOUR GAME.

1294303537

Are you ready to buy?

Find Eaton partner closest to your location

  • UPS systems

What is a UPS and why do gamers need one?

Ever wondered what a UPS is and why it's so important to gamers? A UPS, or 'Uninterruptible Power Supply', is your gaming guardian angel. It protects your precious gaming hardware from the unpredictable world of power outages and voltage fluctuations.

Think of a UPS as your own personal power backup. Depending on its size and the power consumption of your hardware, a UPS can keep your PC running for several crucial minutes during a power outage. If the power failure outlasts the UPS, no worries! Your hardware can be systematically shut down to prevent any loss of data.

But the protection of a UPS doesn't stop at your gaming hardware. It extends to your router too! With a UPS, you'll stay connected and your online gaming experience will be smooth and uninterrupted.

So why do gamers need a UPS? Because in the gaming world, every second counts. And with a UPS, you won't lose a single one to power problems.

eaton-ellipse-pro-range.jpg

Eaton 3S Mini

Designed to keep you connected at all times, the 3S Mini UPS is perfect for gamers. Its super compact, silent, and stylish design blends seamlessly into your gaming setup. With up to 80 minutes for your Internet gateway, 2 hours for your WI-FI extender and 5 hours of battery life for your IP camera, you can enjoy uninterrupted gaming sessions, never missing a moment of action.
Eaton 3S Mini UPS

Eaton 3S Gen2

Stay in the game with the Eaton 3S Gen2 UPS, designed to keep your gaming setup running smoothly even during power outages. This sleek and compact UPS offers reliable battery backup and advanced surge protection for your gaming PC, consoles and other critical electronics. With two USB ports for charging your devices and a sleek design, it fits perfectly into your gaming setup. Mount it on your wall or desk for ultimate space-saving convenience. 
3SGen2 3S850D left

Eaton Ellipse PRO

The Eaton Ellipse PRO is designed to protect your high-performance gaming rig. Featuring a real-time LCD display for instant status updates and measurements, this UPS ensures your system runs smoothly even during power fluctuations. With EcoControl outlets, you can save up to 20% on energy, while Advanced Surge Reduction (ASR) protects your setup from power surges. Its sleek, extra-flat design fits any gaming setup, whether it’s under your desk, mounted on the wall, or in a 19” rack.
Ellipse PRO Range2. Low Res
 
  • Eaton's Tripp Lite Series

Take your gaming beyond 

We all know the thrill of acquiring a powerful PC with top-notch specs. It’s a significant step towards an immersive gaming experience. But is it enough? The answer is a resounding no!

While your PC may be the heart of your gaming setup, it's the peripherals that bring it all together and take your gaming to the next level. Think of it like a symphony - your PC is the conductor, but the music isn't complete without the orchestra.

From monitor mounts that provide the perfect viewing angle, charging stations that keep your wireless devices ready for action, to docking stations that connect your entire setup seamlessly, each peripheral plays a crucial role. They not only enhance your gaming experience but also ensure you’re always at the top of your game.

Consider the cables you use. The right ones ensure high-speed, lossless data transfer for smooth gameplay and stunning graphics. 

So, let’s broaden our horizons beyond just the PC. Let’s dive into the world of gaming peripherals and explore how they can enhance your gaming experience. Because in the quest for gaming excellence, every piece of the puzzle matters.