Download document () of 20

What is the purpose of emergency lighting & how does it work?

Learn about the role of emergency lighting should a threatening event occur. How it delivers peace of mind for buildings owners/operators as well as ensuring compliance.

How emergency lighting functions should power fail, and how it is vital in guiding people to safety when lighting is still present.

What is emergency lighting and why is it required?

Right across the world, environments are becoming increasingly urbanised and intricate, with a corresponding rise in associated safety threats. The challenge is multiplied when a proportion of visitors is not familiar with layout and procedures.

This is the case in large, highly-populated, high-risk or complex premises such as railway stations, shopping centres, airports, stadia, government buildings or leisure facilities – just as it also is in smaller locations with a simpler floor plan.

Emergency lighting is a lifeline in hazardous situations created by this complicated backdrop. Emergency lighting is a lifeline in hazardous situations created by this complicated backdrop. Crucially, it enables the safe, prompt and efficient evacuation of spaces and buildings, not only in cases of blackout caused by power outage but when sunlight and mains lighting may still be available. 

An effective emergency lighting system also guides people in and around enclosed and open environments, as well as helps them locate safety equipment plus refuge and assembly points. By delivering essential illumination and guiding occupants to safe locations and safety equipment, emergency lighting reduces panic and saves lives.

It's about more than peace of mind

However, effective emergency lighting is not only essential for ensuring the peace of mind of those responsible for the safe infrastructure of public and commercial buildings – when six-figure fines and even prison are the price for getting things wrong. It’s also a legal imperative in most countries enforced both by the authorities and insurers. Emergency lighting is heavily governed and defined by product, application and installation legislation standards covering occupational safety and building regulations.

Better by design: The "Green Man" emergency exit sign

One of the most well-recognised icons of emergency lighting is the green running man pictogram design adopted as the international standard ISO 7010 in 1985. It was the winner of a Japanese fire safety association competition in the late 1970s for designer Yukio Ota and has since been adopted and adapted in many countries worldwide.

A design classic, its calm, universal simplicity transcends language barriers making it easily understood. Pictogram-based signs such as this take a cognitive approach and encourage a quicker response from people compared to written instructions.

ISO 7010 emergency exit ESCAPE sign
Recommended signage for progress right EN ISO 7010:2012 E002

The calm, universal simplicity of the ‘green running man’ – a design classic – transcends language barriers to make it quickly understood’

John Robb, Commercial Buildings Director

Emergency exit and safety lighting in action

In just a fraction of a second, the shift from bright, clear mains lighting to total blackout can cause maximum panic and confusion. Exit signs can then support the safe, efficient evacuation of occupants by marking emergency exits, pathways, obstacles and changes of direction.

Escape route lighting also helps reduce panic and identify obstacles during an evacuation in non-blackout scenarios – such as a fire, terror or other security incidents – by ensuring a minimum illumination.

Not all evacuations take place following a power failure or blackout. Emergency lighting plays a vital role in supporting efficient evacuations even in sufficient lighting.

Example of a building during mains lighting conditions

Mains lighting

This corridor shows mains lighting under normal operation in a building.

Example of a building during a blackout without safety lighting

Blackout

A blackout occurs in the building and occupants require direction and light to evacuate the building.

Example of a building with a emergency lighting for escape routes

Blackout with exit sign & safety lights

1. Escape route safety lighting illuminates the floor and helps identify obstacles and safety equipment. It helps avoid panic by ensuring sufficient illumination.

2. Exit signs provide safe and efficient evacuation of all occupants marking emergency exits, pathways and changes of direction.

This way to safety

Get your free emergency lighting fundamentals guide

In our comprehensive guide, we delve deeper into Emergency Lighting design considerations. From conforming to regulations to considering illumination distances and how to combine items to make a complete system.

Start with the emergency lighting leader

Emergency lighting market leader Eaton offers more than 50 years of expertise built up through a brand heritage that embraces CEAG, Luminox, Blessing Menvier, JSB, Crompton and Univel. We work closely with national and international industry organisations to achieve the highest standards of regulatory compliance, safety, reliability and efficiency.