Lataa dokumentti () / 20
We make what matters work*

Data Center Architecture 2025 - Lead and Contact registration

NB! Form is for internal use only!

Contact registration form for all types of Datacenter events: seminars, trainings, customer events, and smaller trade shows.

Lead rating 1: Contacts will flow to Salesforce as leads in 1-2 hours, and they will be assigned to the Finnish lead queue. Comments, Your name and Lead catcher will be passed forward with the lead info.

Lead rating 2: Registration of marketing contacts. Please ask for verbal marketing consent and tick the opt-in checkbox at the bottom of the form.

Navigate back to the lead registration form after submission from the Thank you page.

Contact details of the prospect:


* only required for leads
* only required for leads
Lähettämällä tämän lomakkeen hyväksyn, että antamiani henkilötietoja voidaan jakaa Eatonin, kanavakumppanien ja Eatonin puolesta toimivien kolmansien osapuolten palveluntarjoajien kanssa Eatonin tietosuojakäytännön ja sovellettavien tietosuojalakien mukaisesti.
Yes, customer has explicitly given verbal consent to the Eaton salesperson for sending marketing materials. Marking the checkbox will trigger the double opt-in email to be sent with a link, which the customer would need to click in order to confirm the consent.