문서 다운로드 () / 20
당신의 필요한 일, 이튼이 합니다*

Eaton Magnum Low Voltage Power Circuit Breaker – Quality Campaign

Impacted products

Select Eaton Magnum circuit breakers using mechanical interlocks, key interlocks or internal accessories on the far-right accessory position are impacted.

This includes Magnum, Magnum DS, Magnum SB and IZM (but not including IZMX) circuit breakers manufactured between July 1st, 2017 and March 8th, 2018, as a component or part of an electrical assembly.

If the Magnum circuit breaker configuration in your possession does not use mechanical interlocks, key interlocks, or internal accessories on the far-right accessory position, no immediate action is required.

The primary circuit breaker functions of integral over-current and short-circuit protection, as well as the manual Push OFF button are not affected. The “first” (far left) and “second” (center) accessory positions, and the integral levering interlocks are not affected.

How to identify if your breaker is affected

To verify that your breaker is affected, please refer to the Important Product Safety Bulletin that you have received.

Appendix 1: Helps you to determine if your breaker is in the affected date range.

Appendix 2: Helps you identify potentially affected breakers.

Appendix 3: Helps you determine the factory-installed accessories by catalog number.

Field upgrade action

For customers with select Eaton Magnum circuit breaker configurations using mechanical interlocks, key interlocks, or internal accessories on the 'third' (far-right) accessory position, Eaton resources will be provided to complete the repairs at no cost (Validated GO number required).

To request a list of GO’s that you received with potentially affected breakers, please contact Eaton team MagnumAdvisoryBulletin@eaton.com.

ACTION 1

If you have an affected unit identified by the provided bulletin, please obtain and install the upgrade kit. To start the process, open a warranty claim by contacting the Eaton CORE support group at 1-800-410-2910 or email CORE to CORE@eaton.com.

Claim requirements:

  • Claim type: Request a “Missing Component Claim”
  • Breaker GO and item number: The breaker GO # can be found on the nameplate of the breaker, as shown in Figures 1 & 2
  • Style or catalog number of kit needed: State “2A12888G20”
  • Quantity needed: One kit per affected breaker in your possession
  • Description of the nonconformance: State “Magnum Accessory Lever Field Upgrade“
  • Ship to address for the kits with contact details: Provide the company name, complete shipping address, contact name, and contact email address

ACTION 2

If you are not the end user for this product and have subsequently shipped this product to a third party, Eaton asks that you forward this notice to the third party by registered carrier and assist them in requesting the upgrade kit per ACTION 1.

ACTION 3

If for some reason you are unable to forward this notice to the third party, please contact Eaton team at MagnumAdvisoryBulletin@eaton.com, and request that Eaton contact the end-user. Eaton will need the customer company name, complete shipping address, contact name, and contact email address.