Download document () of 20
We make what matters work*

Substation software applications

Grid design for substations and buildings is a vital part of the overall power system infrastructure assuring constant power supply to consumers. Eaton's substation software solutions provide engineers with the data needed to assure installations are optimized for operation, connection and protection.  

Developing effective grounding grid design

The CYMGRD software assists the engineer in designing the grounding grids and performing soil resistivity measurement interpretations, elevation of ground potential rise and danger point evaluation within any area of interest.

Efficient, effective designs made easy

User-friendly data entry and powerful analysis algorithms make the CYMGRD software an efficient tool that helps engineers arrive at technically sound and economical designs.
Specifications

Substation grounding

Analytical capabilities

Engineers require powerful analysis tools when they are called on to optimise the design of new grids and reinforce existing grids.
 

Find out more about analytical capabilities

CYMGRD/AutoCAD interface module
 

Eaton's CYMGRD/AutoCAD Interface module allows the user to alternate between the AutoCAD and the CYMGRD environments. 

This utility is not a substitute for AutoCAD. In fact, AutoCAD remains a firm software requirement, because it is AutoCAD that will produce the necessary *.DXF or *.DWG file(s) that contain the pictorial description of the substation grid layout realised with the CYMGRD software.

Find out more about CYMGRD/AutoCAD interface module

Power system analysis and modelling

Network editor

The Network editor features a user-customisable graphical user interface underlying the CYMDIST applications and the complementary CYME analyses modules.

This includes extensive modelling capability of distributed energy resources (DER) equipment and energy storage; along with the definition of all customer types necessary. The software also includes control models that are relevant to the various generation sources. All libraries can be enriched by users.

The network editor is included in the Distribution System Analysis package (CYMDIST).

Find out more about the network editor module

Enhanced substation modelling

This module enables the accurate representation of all the major components of a distribution substation, as well as  any sub-network, such as a vault, a switching cubicle or an industrial facility. The simulations then take into account the effects of these installations on the overall distribution system.

Find out more about the enhanced substation modeling module

Fault analysis

Ensure system safety by assessing the effects of short-circuits (conventional, ANSI, IEC 60909 and IEC 61363), series and simultaneous. Locate faults, verify equipment ratings and study voltage sags.

Find out more about the fault analysis module

Protective device analysis

This module helps power engineers effectively address protection issues by analysing time-current curves. The library contains over 15,000 protective device curves.

Module features: network protection analysis, minimum fault analysis and sequence of operation.

Find out more about protective device analysis

Arc-flash hazard analysis

Properly assess the arc flash risk level to ensure a safer work environment by computing the necessary parameters required to determine risk level and adopt adequate safety procedures. This includes a new method that factors in back-up protection, multiple contribution and duration.

Find out more about the arc-flash hazard analysis module

Download Links
X
Download Close