Select your location

Fuses made simple (control circuits)

The easiest and fastest way to select and specify the right control circuit fuse

Bussmann’s Fuses Made Simple program provides the easiest and fastest way to select and specify the right fuse. Whether it’s branch circuit or control circuit (supplemental) fuses, we take the guesswork out of selecting the right fuse. What’s more, we make it simple to replace fuses with six color groups (categorized by voltage rating)--all while enhancing the safety of the electrical system.

Find the control circuit fuse you need in three simple steps:

1. Type

Select the fuse type. Select from time-delay (for inductive loads) or fast-acting (for resistive loads).

2. Voltage

Select the voltage rating needed. Keep in mind that fuse voltage rating must be equal to or greater than the circuit voltage.

3. Interrupting Rating

Verify that the interrupting rating of the fuse selected is sufficient for the circuit application. Keep in mind that the interrupting rating must be equal to or greater than the available short-circuit current.

Product Profile # 10225

Brochure # 10223

Use the table below to find and select the right control circuit fuse, click on the fuse family for product details.

Fuses Made Simple control circuit fuses

Fuse Type Maximum Voltage Rating Fuse Family Color Code Amp Range Interrupting Rating
Time-delay 600Vac Recommended using Low-Peak LP-CC Class CC fuses*
500Vac FNQ Orange 1/10 to 30A 10kA
250Vac FNM Green 1/10 to 1A 35A
FNM Green 1-1/8 to 3-1/2A 100A
FNM Green 4 to 10A 200A
FNM Green 12 to 30A 10kA
FNA(2) Green 1/10 to 8/10A 35A
FNA(2) Green 1 to 6A 200A
125Vac FNA(2) Blue 6-1/4 to 15A 10kA
48Vac Upgrade to 125Vac
  32Vac FNA(2) Grey 20 to 30A 1kA
Fast-acting 600Vac KTK Black 1/10 to 30A 100kA
KLM(3) Black 1/10 to 30A 100kA
BBS(1) Black 1/10 to 6A 10kA
500vac Upgrade to 600Vac
250Vac BAF Green 1/4 to 1A 35A
BAF Green 1-1/2-3A 100A
BAF Green 4-10A 200A
BAF Green 12-15A 750A
BAF Green 20-30A 200A
BBS(1) Green 7-10A 10kA
MIC(2) Green 1A 35A
MIC(2) Green 2-3A 100A
MIC(2) Green 5-10A 200A
MIC(2) Green 15A 750A
125Vac Upgrade to 250Vac
48Vac BBS(1) Purple 12-30A **
32Vac
MIC(2) Grey 20-30A 10kA

For ultimate protection, any of the control circuit fuses above can be upgraded to a branch circuit Low-Peak LP-CC Class CC fuse.*

1. Fuse is 1-3/8” long.
2. Fuse is pin indicating.
3. Fuse is also rated for 600Vdc, 50kA interrupting rating.
* For primary protection of control transformers, use FNQ-R.
** For interrupting rating, contact factory.

Importance of voltage rating and interrupting rating

Control circuit fuses have many different voltage ratings, ranging from 32Vac to 600Vac, and interrupting ratings up to 100kA. Because their physical size does not vary with voltage or interrupting ratings, the most frequent cause of misapplication is due to improper voltage or interrupting rating selection. This leads to compromised system integrity, and equipment and personnel safety. It is important to note, though, that when a fuse is applied beyond its ratings, there may not be any initial indicators. Adverse consequences typically result when a system fault occurs and an improperly sized fuse attempts to interrupt an overcurrent event.

Voltage Rating

Voltage rating is extremely important. The proper application of an overcurrent protective device, according to its voltage rating, requires that the voltage rating of the device be equal to or greater than the system voltage.It can be higher but not lower. For instance, a 600V fuse can be used to safely protect a 208V circuit. However, when an overcurrent protective device is applied beyond its rating, there may be potential for fire and arcing energy, which poses a severe fire risk to other components in the panel.

Interrupting Rating

Interrupting rating is also of critical importance. An overcurrent protective device must be able to withstand the destructive energy of short-circuit currents of the equipment it is protecting. If a fault current exceeds a level beyond the capacity of the protective device, the device may actually rupture, causing additional damage. It is therefore important when applying a fuse to use one that can sustain the largest potential short-circuit currents. Failure to apply fuses with the appropriate interrupting rating can be a serious safety hazard.

Fuses Made Simple™ - Control Circuits helps enhance safety

Bussmann's Fuses Made Simple - Control Circuits helps minimize the risk of misapplication by clearly and consistently indicating both the voltage rating and interrupting rating on the fuse label. The voltage rating is easily identified by both the color code band and the large print on the fuse label. Additionally, the interrupting rating is printed on the side of each fuse.

Fuses Made Simple™ - Control Circuits helps enhance safety

Bussmann's Fuses Made Simple - Control Circuits helps minimize the risk of misapplication by clearly and consistently indicating both the voltage rating and interrupting rating on the fuse label. The voltage rating is easily identified by both the color code band and the large print on the fuse label. Additionally, the interrupting rating is printed on the side of each fuse.

Simple Replacement

Color-coded by voltage

Each fuse label has a unique identifying color band that represents the fuse’s maximum voltage rating. When it’s time to replace a fuse, Bussmann makes it easy to search for the replacement. Select the voltage needed by simply looking for the Bussmann fuse with the right color band in the storage bin. This narrows the search and speeds replacement time.

  • 600Vac - Black  (KTK, KLM BBS)
  • 500Vac - Orange (FNQ)
  • 250Vac - Green (FNM, FNA2, BAF, BBS1, MIC2)
  • 125Vac - Blue (FNA2)
  • 48Vac - Purple (BBS1)
  • 32Vac - Grey (FNA2, MIC2)

1. Fuse is 1-3/8" long.

2. Fuse is pin indicating.

3. Fuse is also rated for 600Vdc.

Consistent look for each label

Every fuse label now has a consistent look. Critical fuse information is presented in an easy-to-read format across the entire Bussmann control circuit fuse portfolio to help speed replacement.