If you would like to add or change the scheduling options, please follow these steps:
You can set up your EV charger to charge your EV at a specified time. You can have one schedule for weekdays and another for weekends.
To select a charging schedule, you need to disable the "All day" option:
The app allows you to set up EV charging hours, as well as the charging power, for both weekdays and weekends.
Enter a start and end date to define your EV charging schedule. Note that if you are using the load-balancing feature, the scheduling will not be possible.
If you want to reduce the charging power of your EV charger, you can use the slider control and set the power limit to a preferred value.
This option is available for all charging modes: Protected EV Charging and Automatic EV Charging (weekdays and weekends).