Download dokument () af 20

Eaton Introduces the Next Generation Curved WaveStream LED and LuxWire Technologies

Date: March 14, 2017

PEACHTREE CITY, GA — Power management company Eaton announces the launch of the Neo-Ray Covera and Converge architectural suspended product families featuring its new next generation curved WaveStream light-emitting diode (LED) technology. Combining a contemporary and minimalist design with advanced optical performance and connected lighting capabilities, the two pendant families also introduce Eaton’s LuxWire technology, allowing the luminaires to suspend effortlessly in space without large, unsightly power cables. 

“The new curved WaveStream technology delivers the same precise optical performance as our planer WaveStream solutions, and combined with the LuxWire technology, offers specifiers a unique, sophisticated and elegant suspended ambient illumination solution,” said Tim Bingaman, general manager, Neo-Ray. “By adding our enabled or connected lighting solutions, customers can save on installation and operating costs, reduce maintenance costs and increase overall energy savings.”

Eaton’s patented WaveStream LED technology features laser-precise AccuAim optics arranged in exacting patterns to provide unparalleled brightness control, while delivering optimal distributions tailored to each fixture and application. 

The advanced LuxWire technology delivers low-voltage power to the luminaires through the same aircraft cables from which it’s suspended, allowing drivers and bulky power cords to be placed above the ceiling.

The Neo-Ray Covera product family offers a variety of scalable and flexible design solutions, integrating seamlessly into any commercial or high-end residential space. Available in 2- or 4-foot lengths with a variety of mounting options and lumen packages, the curved optical design enables designers to use the luminaire in a variety of applications from task and decorative lighting to ambient lighting in an open office environment. Unique to the Covera luminaires, custom finishes options include of selection of three standard and six architectural hydrographic finishes, to help enhance spaces. 

Eaton’s Converge LED suspended family is available in 4- and 8-foot individual luminaires and for continuous runs, in 4-foot increments, with a variety of mounting options. For added design flexibility, the luminaires are offered in both curvilinear and rectilinear profiles. Designed to provide the highest degree of visual comfort while maximizing energy efficiency, the Converge’s uplight distribution provides ideal ceiling uniformity, allowing lighting
designers and specifiers to increase row spacing regardless of the suspension length. By increasing luminaire row spacing, the total installed lighting cost and the overall watts per square foot is reduced.

Many interior spaces are vacant during off-peak times, remaining fully illuminated, wasting energy and shortening the life of the system. To maximize operating efficiency and overall savings, while driving down maintenance and installation costs, Eaton offers integral 0-10V dimming drivers as standard and a wide range of enabled and connected lighting options, allowing the lighting to be controlled by external systems or an optional FifthLight DALI driver to enable addressable digital control. 

In addition, the Covera and Converge products are available with Eaton’s connected lighting solutions. The Distributed Low-Voltage Power (DLVP) System simplifies energy efficient code compliance and streamlines installation, reducing the total installed cost of a lighting with controls project by up to 20 percent. Eaton’s LumaWatt Pro Connected Lighting System powered by Enlighted, allows customers to reduce energy costs, improve occupant comfort and establish a unified solution for energy management and building automation. The system allows users to take advantage of the advanced Internet of Things (IoT) capabilities to acquire actionable, granular data on lighting energy use and performance, space utilization, asset tracking, HVAC and more.

For more information, visit www.eaton.com/covera and www.eaton.com/converge

Eaton delivers a range of innovative and reliable indoor and outdoor lighting solutions, as well as controls products specifically designed to maximize performance, energy efficiency and cost savings. Eaton lighting solutions serve customers in the commercial, industrial, retail, institutional, residential, utility and other markets. 

Eaton’s electrical business is a global leader with expertise in power distribution and circuit protection; backup power protection; control and automation; lighting and security; structural solutions and wiring devices; solutions for harsh and hazardous environments; and engineering services. Eaton is positioned through its global solutions to answer today’s most critical electrical power management challenges.

Eaton is a power management company with 2016 sales of $19.7 billion. We provide energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton is dedicated to improving the quality of life and the environment through the use of power management technologies and services. Eaton has approximately 95,000 employees and sells products to customers in more than 175 countries. For more information, visit Eaton.com.

Contact US 
Karin Martin, (847) 754-5699
Ann Marie Halal, (440) 523-4418