Download dokument () af 20

White paper

Update of the ERP guideline (EG) 640/2009

Successfully increase energy efficiency in drive technology

Electric drives account for around 70% of total electricity consumption in industry. It is estimated that by 2020 electric motors in Europe will convert 1,470 TWh of electricity into mechanical energy. Alone through previous Regulation (EC) 640/2009, it is estimated that energy savings of 102 TWh will be achieved by 2030 per year.

The regulation will now be continued by the follow-up study Lot 30 "Ecodesign Requirements for Motors and Variable Speed ​​Drives": this will lead to an additional, estimated electricity saving of 10 TWh per year. The new regulation comes into force in two stages: step one 1.7.2021 and step two 1.7.2023. What the new regulations mean for the industry in detail, and which design possibilities with energy-efficient motors, motor starters, soft starters and variable frequency drives users have to achieve their energy efficiency goals, is described in the white paper.

eaton-update-erp-guidelines-cover-picture-WP040007en
Ved at indsende denne formular accepterer jeg, at de personlige data, som jeg giver, kan deles med Eaton, kanalpartnere og tredjepartsudbydere på vegne af Eaton i overensstemmelse med Eatons privatlivspolitik og i overensstemmelse med gældende databeskyttelseslovgivning.
I agree to be informed regularly about Eaton products, promotions and news. I understand and agree that Eaton will use my data to personalize marketing communications. Any use of my personal data will take place in compliance with the relevant and applicable data privacy laws and the  Eaton Privacy Policy. I can withdraw my consent to receive marketing communications at any time by contacting Eaton.