Download dokument () af 20
Eaton-blog-EE-pump-systems.jpg

Whether they are used as a supercharger in heat pumps or in the pumping station of a waterwork, pumps are among the largest industrial consumers of electricity. Based on the life cycle of a pump, the energy costs average around 45% of the total costs.

How much energy can be saved when it comes to pumps?

A significant amount of energy can potentially be saved in pump systems, not least because they are generally operational in the partial load range. According to the German Federal Ministry for Economic Affairs and Climate Action, the energy consumption of pump systems can be reduced by 30% through a combination of energy-efficient technologies and process optimization.

icon_Linkedin_colored_256x256.png

Follow #EatonMachine on LinkedIn

Get every important blog post or new information Eaton is pulishing for machine and systembuilders. 

Which components of a pump system must be taken into account when optimizing energy consumption?

Modern pump systems generally consist of a motor, a motor control, and the actual pump, as well as valves, actuators, and accessories such as sensors, hoses and filters.

Each of these components must be considered when thinking about increasing energy efficiency. When it comes to motors, the efficiency rating according to the IEC 60034-30 standard should be considered (efficiency class/IE = International Efficiency). Efficiency is rated in four classes:

  • IE1 (Standard Efficiency)
  • IE2 (High Efficiency)
  • IE3 (Premium Efficiency)
  • IE4 (Super Premium Efficiency)

What are typical combinations of components in pump systems?

In industrial facilities, different combinations of components are used in pump systems.

eaton.blog-energy-efficiency.31798 Diagram 2
The overwhelming majority of pump systems currently in use work with a motor and fixed displacement pump at a constant speed. The pressure and rated flow are regulated by hydraulic valves. The investment costs for this solution are relatively low, but the energy consumption is high: The entire system is designed for the maximum required pressure and rated flow and supplies this amount of power even when it is not needed.
eaton-blog-energy-efficiency-blog7-aggregat
The high-end solution is the four-quadrant direct drive (servo solution). A servo drive precisely regulates the speed, and therefore the pressure and rated flow. Valves and throttling points for controlling the actuators are no longer necessary. The drive only runs at the power level that is actually required by the system.
eaton-blog-energy-efficiency-diagram-3

The basic approach behind power-on-demand systems is to operate the pump in a way that varies depending on the process and the power that is actually required, rather than using a constant speed. Speed-controlled pumps of this kind only consume energy when the system is actually generating power (power on demand). This means that heat dissipation is reduced significantly and effectively.

 

How is a speed-controlled pump implemented?

A power-on-demand system can be implemented with a conventional asynchronous motor. Depending on the operating cycles and running times, motors in efficiency classes IE2 to IE4 are used. Either a variable speed starter or a variable speed drive can be used for speed control.

The motor control receives data from a pressure sensor about the pressure in the hydraulic system and adjusts the motor speed to the required rated flow accordingly. This system also makes it possibly to supply several parallel processes that have similar requirements for rated flow and pressure. The various actuators can be controlled via directional, proportional or servo valves.

eaton-EE-blog7-figure1

Advantages of power-on-demand systems

Application example: Waterworks

Three clean water pumps in a waterworks owned by the Stauden-Wasserversorgung water utility company were powered by conventional electric motors at 55 kilowatts of power each, all activated via motor starters. With this drive technology, the pumps could not operate at their optimum operating point, i.e., in the most energy-efficient manner – the pumps either did not run at all or ran at full power.

Aquatech replaced the conventional electric motors with IE4 motors, which are particularly energy-efficient. In addition, speed-controlled operation was introduced for the motors. The motor starters were thus replaced with PowerXL DG1 variable speed drives from Eaton.

All in all, the combination of IE4 motors with the DG1 drives enabled the Stauden-Wasserversorgung water utility company to cut the energy costs of the pump system by about 15 %.

What are the other elements of an energy-efficient pump drive?

Reducing the energy consumption of a pump system is the first step towards creating an energy-efficient system. The second step is to pave the way for an energy management system. The key principle here is data acquisition: Only by comprehensively recording and analyzing data relating to energy and machines is it possible to review energy consumption, identify opportunities for optimization and monitor the effects of any measures that are implemented.

An intelligent connection system at device level, such as Eaton’s SmartWire-DT, offers significant advantages here. Such systems mean that components such as switchgear, circuit breakers, pilot devices and actuators can be connected to the controller via a single wire instead of time-consuming point-to-point wiring being required.

Conclusion

Speed-controlled, electro-hydraulic drives are intelligent drive systems that offer an optimal system solution for increasing the energy efficiency of pumps in many applications. They not only help to protect the climate and save energy, but also lower the total cost of ownership (TCO).

Although the investment costs are higher than those of conventional pump systems, these are offset by lower energy costs and shorter payback periods. A further benefit stemming from the fact that they operate based on requirements (power on demand) is that more compact systems can be implemented. In turn, these have lower cooling demands and reduced sound emissions. Speed-controlled pump drives make it possible to achieve significant energy savings with relatively low investment costs – a reduction in energy consumption of up to 70 % has already been achieved in practice.

More detailed information is available in Eaton’s white paper “Planning and operating hydraulic power units to provide greater energy efficiency”, which is available for download on the company’s website.

 

White paper informs how to increase energy efficiency of pumping applications

Electrical and mechanical components such as drives, pumps and valves are typically combined in order to implement control tasks in fluid-power applications. The question of which elements are used, and how they are integrated into the system, has a decisive influence on the energy consumption of the overall solution. The white paper explains the reasons for, and approaches to, reducing energy consumption, and presents practical application examples.
PowerXL DA1 Variable Frequency Drives
PowerXL DA1 Variable frequency drive
PowerXL DM1 micro VFD
PowerXL DM1 Variable frequency drive
DG1-345D6EB-C20C_R.jpg
PowerXL DG1 Variable frequency drive