Descargar documento () de 20

CHANHASSEN, MN, USA … To ensure the safe operation of hydraulic systems, lubricants and hydraulic oils must be protected from unwanted particles. With hydraulic and lubricating oil filters from Eaton, operators are able to protect their machinery and maximize its operating potential through long service-life. Tank mounted filtration solutions are now complemented by the BR210 Dirt-Gate™ and BR110 H2O-Gate™ vent breathers, expanding the functionality of the product range.

Both BR series filters boast high efficiencies and minimal pressure drop, effectively removing abrasive particles from the air before they can enter the hydraulic tank. This protects the hydraulic system from external contamination and significantly extends the fluid life.

With the BR110 H2O-Gate vent breather, Eaton introduces an additional variant that further expands the functions of the product range. “While it remains in the tank, hydraulic oil degasses, releasing oil particles into the air,” explains Simone Ortner, Engineering Manager of Eaton’s Filtration Division. These particles may pose a health risk and also pose a safety risk in hazardous environments (Ex zones). “The BR110 vent breather helps mitigate these risks,” Ortner continues. “Because of its unique ability to breathe, the BR110 not only protects the hydraulic oil from contamination, the filter also inhibits oil particles from escaping into the environment.” Additionally, the BR110 vent breather ensures that no moisture enters the tank, minimizing condensation and optimizing hydraulic oil performance through continuous air exchange.

 

Eaton's BR series of vent breathers feature a durable plastic housing that protects the filter media from external influences. The filters are temperature resistant up to 250°F (121°C) and offer a nominal output of up to 25 CFM (708 l/min). A visual mechanical indicator actuates when the filter capacity is exhausted or the media has become clogged.

From heavy commercial vehicles to agriculture, and across various mobile applications in industries such as chemicals and oil and gas, Eaton's BR series filters are used to protect machinery and equipment from corrosion and wear. With the BR110 vent breather, operators now meet the most demanding requirements for air quality while optimizing the performance of their hydraulic fluids.

eaton-br110-br210-vent-breather.jpg
Eaton's BR series of vent breathers protect hydraulic systems from airborne contaminants. The BR110 H2O-Gate vent breather additionally reduces the moisture in the hydraulic tank and inhibits hydraulic fluid particles from escaping into the ambient air.

About Eaton’s Filtration Division:

Eaton’s Filtration Division is a leader in liquid filtration that can help companies improve product quality, increase manufacturing efficiency, protect employees and equipment, and help achieve sustainability goals. Eaton employees around the world make a difference for their customers by creating an exceptional customer experience, solving problems with application expertise and developing innovative filtration solutions. Eaton’s filtration products are manufactured and sold worldwide. For more information, visit Eaton.com/filtration.

Eaton is an intelligent power management company dedicated to protecting the environment and improving the quality of life for people everywhere. We make products for the data center, utility, industrial, commercial, machine building, residential, aerospace and mobility markets. We are guided by our commitment to do business right, to operate sustainably and to help our customers manage power ─ today and well into the future. By capitalizing on the global growth trends of electrification and digitalization, we’re accelerating the planet’s transition to renewable energy sources, helping to solve the world’s most urgent power management challenges, and building a more sustainable society for people today and generations to come.

Eaton was founded in 1911 and has been listed on the New York Stock Exchange for more than a century. We reported revenues of $23.2 billion in 2023 and serve customers in more than 160 countries. For more information, visit www.eaton.com. Follow us on LinkedIn.

Contact
Uta Hilgers
+49 6704 204 204