문서 다운로드 () / 20
당신의 필요한 일, 이튼이 합니다*

Power management FAQ

Whether you’d like to monitor a single uninterruptible power supply (UPS), integrate with leading virtualization platforms or manage an entire data center, cutting-edge connectivity options cannot only enhance your business continuity, but can significantly slash your operating expenses, reduce infrastructure requirements, and boost productivity and responsiveness even during a prolonged outage. Check out this FAQ to learn more about power management software and network connectivity. 

Need help determining the best power management solution for you?

Why is monitoring and managing your power infrastructure important?

Power outages take a toll on businesses of all sizes, across every industry. That’s why it’s important to safeguard your IT equipment with a power management solution that can keep your critical applications always-on during interruptions. Monitoring and management software is the perfect complement to your uninterruptible power supply (UPS) and power distribution unit (PDU) devices. There are a range of options on the market today, from a basic network connectivity cards to multiple software platforms. 

Regardless of your location, you can receive advanced alerts from afar, trigger advanced actions like migrating virtual machines, and make data actionable through faster, scalable interpretation.

Why is a UPS not enough?

Although UPSs are typically rugged and reliable, they do require ongoing monitoring and support.

Connected devices allow you to continuously monitor and diagnose the state of your environment, batteries and power sources, along with the condition of the UPS’s internal electronics.

There is a shift in the IT industry; professionals are focusing on more secure and reliable remote site management, making it necessary to monitor network devices remotely—anytime from anywhere.

With a network card, you can securely monitor and control an individual UPS by connecting it directly to the network. Its features keep you informed of problems as they occur, ensuring uptime in the event of an extended power outage.

What is a network connectivity card?

Network cards allow for secure monitoring and control of an individual UPS by connecting it directly to the network.

This connectivity is the conduit for your device’s data and information, providing status, alerts and remote capabilities. The notification features keep you informed of problems as they occur, avoiding shutdown in the event of an extended power outage, always keeping your business information safe.

Did you know?

Software-defined power is the continuous management of power via virtualization platforms and disaster recovery techniques to optimize power and cooling consumption, and ultimately save users money, improve operational flexibility and avoid unplanned downtime.

What are the different remote communication card types?

  • IT-based: SNMP enables your unit to be accessible via the internet to monitor the software
  • Facilities: Modbus, BACnet, SNMP
  • Relay: Provides alarm and health status of your UPS through relay contacts

Can network connectivity devices monitor physical environments?

Yes, environmental monitoring probes (EMP), such as the Eaton EMP Gen 2, are connectivity devices that enable you to collect temperature and humidity readings in the rack environment and monitor the environmental data via the onboard LCD screen or remotely using a Telnet connection or standard web browser. You can also monitor the status of two contact closure devices, such as door switches.

How can you reduce your cybersecurity risk?

Eaton’s Gigabit Network Card is the first in the industry to receive UL 2900-2-2 certification, ensuring it has been reviewed and tested, and meets the benchmark of this trusted brand. Encryption and password management are two key enhancements included in the Gigabit Network Card.

Password management:

  • Requires change of password on setup
  • Configurable requirements for password complexity
  • Certificate based authentication in machine to machine connections— no username/password information saved on the client machine, separate certificates for each protocol

Encryption:

  • Uses the most current version of Transport Layer Security protocol (TLS)
  • Only secure protocols enabled by default
  • Firmware is signed and encrypted, and will not boot if tampered with
  • Secure SMTP for email alerts

What are some of the benefits of power management software?

For you to get the most out of your network connectivity hardware through analysis software platforms, first consider the value of reporting. Custom reports can analyze your data and identify trends, while providing capacity planning and deployment recommendations.

The Eaton Intelligence Platform works to automate, monitor, visualize and predict these problems before they strike. Whether your IT environment is a small deployment of UPS units and rack PDUs, a sophisticated data center housing thousands of servers and millions of datasets, or anything in between, our platform is versatile enough to adapt with you. 

Our platform is ready to take on the unique challenges you face within your environment, by empowering you to:

Find out which power management solution best fits your IT environment.

In what ways are network cards a higher investment than Peripheral Component Interconnect (PCI) cards?

UPS and PDU network cards are like small computers. It’s not the cost of the materials that drive the price but rather the engineering and development required to make sure the card is compatible with network communication protocols and various operating systems. You get the luxury of all the application features and accessories built into one network card, linked with security. 

Why aren’t network cards automatically included with every UPS?

Not every user wants or requires a network card and including a network card would increase the price of the UPS. This is because all the application features and accessories are conveniently built in to the network card, allowing for better security and overall, a better investment.

Want to learn even more about power management software and connectivity?