Document downloaden () van 20

Tested in practice

50% faster wiring with Push-in technology

The Push-in technology offers machine builders and system integrators a number of advantages. First and foremost, the technology simplifies the wiring of switchgear and saves time: The ferrule-terminated cable simply has to be plugged into the terminal blocks, which can be done with one hand and without any tools. This is why Eaton also equips its PKZM0 and PKE motor-protective circuit breakers, DIL M contactors and DIL A contactor relays with Push-in technology. 

Customer interview

In the run-up to the market launch, we conducted a field test together with Hanseatic Power Solutions GmbH (HPS for short) to determine the actual productivity benefits during the wiring process. 

HPS designs and manufactures switchgear and control systems for a wide range of sectors – including industrial, building, marine and off-shore applications. The company’s portfolio ranges from simple emergency power supply control equipment to complete electrical systems for power stations.

HPS, which is based in northern Germany, employs 85 people, operates worldwide and also has a branch in Abu Dhabi. To date, the company has been using various products from Eaton's portfolio, such as the PKZ and PKE motor-protective circuit breakers with screw terminals and the DIL A and DIL M contactors with screw and spring-loaded terminals. For the wiring of these switching devices and accessories alone, four different torques need to be taken into account. 

eaton-hanseatic-power-solution-bernd-mähnss.jpg
Bernd Mähnss, Managing Partner of Hanseatic Power Solutions GmbH, explains the results of the test
eaton-push-in-efficient-working-with-two-hands.jpg
With tool-free assembly, the technician can hold several cables in one hand and then plug them in one after the other using the other hand, which is one of the reasons for the considerable time savings.

Mr. Mähnss, what was your motivation to take part in this test?

We have been using Eaton devices since 2009, initially those with conventional screw technology, then partly switching to cage clamps and finally to Push-in technology. At first, we only used Push-in connections for terminal blocks, but then we added more and more devices. Now we are about to make the switch for Eaton contactors as well. The test gave us the opportunity to find out in advance how much time we can really save with Push-in technology during production.

Is time a critical factor for you?

Of course! The longer it takes our employees to wire the switchgear, the more expensive it becomes. And the easier we make the wiring work for our staff, the faster we can deliver the system. Every minute, every hour is money.

What are the most important results of the test for you?

Compared to screw terminals, we were able to demonstrate average time savings of around 50 percent for Push-in connections. What surprised us, however, was the time saved in comparison with spring-loaded terminals, where we also identified considerable time savings of around 40 %.

That's actually quite a lot, given that spring-loaded terminals are already considered a more efficient connection technology. How do you explain these time savings?

The explanation is relatively simple: In the case of spring-loaded terminals, opening the connection requires a slotted screwdriver. This means that I have to hold the conductor in one hand, and the tool needed to connect it in the other. With Push-in technology, I don't need any tools, enabling me to hold several conductors in one hand at the same time, which I can then plug in one after the other using the other hand – which saves a lot of time. 

hourglass-teal-icon

50% time saving

Apart from these time savings, what other advantages do Push-in connections offer?

For one, they provide greater safety during wiring: Especially when connecting larger devices, selecting the right torque for the screw terminals can be a problem. If the selected torque is too low, fires may easily occur during live operation. During testing, these errors are not necessarily noticeable due to the low test current, but if the terminal is subjected to the maximum current during operation, it may burn to a crisp. Push-in terminals completely eliminate this risk. With Push-in terminals, there is also no longer the risk of excessive torque, meaning there is no danger of the screw head being torn off. 

eaton-push-in-technology-cables-dark.jpg
Previously, if this happened, the entire device would have to be replaced. Push-in connections also offer an advantage during the initial check to see whether the conductors are loose. Already during the connection process, this check can be carried out with a single movement of the hand: Simply pull the conductor briefly after plugging it in – and you'll know whether it is secure. This is a workflow that the test facility staff also quickly became accustomed to. In addition, carrying out this check is also easier than in the case of screw terminals, since Push-in terminals are connected at the front. Screw terminals, on the other hand, still need to be pulled into the cable duct from above or below, which is a bit more time-consuming. And last but not least, it can also be an advantage to work with Push-in connections on construction sites, where the space available for installation may be a little tight for screw terminals. Push-in terminals also offer additional benefits in this respect, as there is no need to handle any tools and the cables simply have to be plugged in at the front.

Is it fair to say then that the significantly greater efficiency of the wiring process also helps to combat the shortage of skilled workers?

That is indeed the case. In the course of digitalization, the workload is shifting away from purely manual tasks such as wiring to new technologies such as the creation of digital twins, the routing of cables via software, and so on. If our well-trained staff needs less time to wire the systems by using the tested Push-in technology, we can invest more time in the preparatory work, which in the end means quality improvements thanks to better planning.

If you now replace all devices equipped with screw terminals with Push-in products – what efficiency gains will that bring?

We have already been using Push-in terminal blocks and control relays for some time. In combination with prefabricated cable harnesses, which are labeled with the target designation, we can achieve time savings of up to 50 % during assembly and wiring.

What is the level of acceptance of Push-in technology across different industries - are there any reservations?

No, there aren’t. We also use Push-in connections in marine technology, for example. Most companies and certification bodies have no problems with Push-in technology.

In your experience, how does Push-in technology perform in terms of vibration resistance?

Until now, our switchgear with Push-in connections has never come loose, not even during shipping. Even though customers should always check all connections prior to commissioning, regardless of whether Push-in or screw terminals are used, the risk of any parts coming loose during transport is much lower with Push-in terminals.

Does this mean that you will soon be switching completely to Push-in technology?

That's right, as soon as the Eaton devices with Push-in connections come onto the market – which is currently planned for summer 2021 – we will implement the change.