Download document () of 20

Eaton's LED Luminaire Offers a Versatile, Energy-Saving and Affordable Solution for Area, Site and Roadway Applications

November 23, 2015

PEACHTREE CITY, GA … Power management company Eaton today announced the introduction of its Lumark Prevail light-emitting diode (LED) Luminaire, a versatile, energy-saving and affordable lighting solution for area, site and roadway applications. Featuring a patent-pending architectural design, the Prevail luminaire combines easy installation features with multiple controls options, resulting in significant installation, energy and maintenance savings for both retrofit and new applications.

“The Lumark Prevail luminaire can provide energy and maintenance savings of more than 60 percent when compared to traditional metal halide products, qualifying the fixture for energy rebates,” said Kraig Kasler, president, Eaton’s Lighting Division. “The variety of controls solutions include an optional Integrated Sensor Control System that offers occupancy detection and daylight harvesting, providing additional energy and installation savings, while complying with some mandated energy code requirements.”

In addition to the Integrated Sensor Control System, the Prevail luminaire is available with Eaton’s additional control features including an optional LumaWatt Outdoor Wireless Control and Monitoring System, which manages the lighting levels according to pedestrian and traffic safety needs. The system allows for metering power consumption and wireless communication and employs four control strategies to automate luminaire behavior including scheduled on/off, scheduled dimming, occupancy detection and daylight harvesting. The product is also offered with an optional National Electrical Manufacturers Association 3-pin or 7-pin photocontrol receptacle, enabling wireless dimming when used with a compatible photocontrol.

The Prevail luminaire’s patent pending, standard versatile arm mount makes retrofit and new installations easy. The standard arm, which features a built-in wiring compartment for simple installation, can also uniquely accommodate a wide range of existing fixture drilling patterns and can be installed on both square and round poles, simplifying and reducing installation time and cost. The fixture is also available with a wall and mast arm for building and roadway applications.

Featuring Eaton’s patented LED optical technology, the luminaire is offered in four optical distributions that deliver controlled, uniform illumination and maximum light levels, directing the light exactly where it’s needed. A low profile, modern architectural design allows one housing to accommodate multiple lumen packages ranging from 6,100 to 15,100 nominal lumens to replace typical high intensity discharge (HID) products from 150 watts to up to 400 watts.

Besides its performance, the Prevail LED luminaire is engineered for long-term reliability.
With lumen maintenance greater than 92 percent at 60,000 hours, the rugged, die-cast fixture housing is 3G vibration and IP66 rated, which provides years of operation with minimal service requirements for area lighting applications including parking lots, walkways, roadways and building areas in commercial and industrial applications.

To learn more about Eaton’s lighting solutions, visit www.eaton.com/lighting.

Eaton delivers a range of innovative and reliable indoor and outdoor lighting solutions, as well as controls products specifically designed to maximize performance, energy efficiency and cost savings. Eaton lighting solutions serve customers in the commercial, industrial, retail, institutional, residential, utility and other markets.

Eaton’s electrical business is a global leader with expertise in power distribution and circuit protection; backup power protection; control and automation; lighting and security; structural solutions and wiring devices; solutions for harsh and hazardous environments; and engineering services. Eaton is positioned through its global solutions to answer today’s most critical electrical power management challenges.

Eaton is a power management company with 2014 sales of $22.6 billion. Eaton provides energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton has approximately 99,000 employees and sells products to customers in more than 175 countries.