Download dokument () af 20
We make what matters work*
  • Grid modernization software applications

    Eaton’s CYME advanced software applications provide enhanced grid reliability and security for deploying decentralized energy sources and smarter devices in the planning and operation of electric utilities.
    Want to know more

Core features

  • Distribution system analysis includes all generation sources
  • Powerful algorithms for efficient analysis
  • Identify and isolate probable faults during planning
  • Additional modules support advanced simulation of the entire network
  • Analyze implementation scenarios, risks and costs associated with modernization projects

Design and modelling

Defining the types of customers and loads on the system and specifying the various generation models is the cornerstone of a complete, accurate analysis. Eaton's CYME software supports modelling of new devices, power sources, microgrids, power electronics and storage.

Powerful distribution system analysis

As power systems transition to two-way flow systems, accurate analysis must include all generation sources. Eaton’s CYME software algorithms provide an efficient means for creating accurate system analyses.

Meet the challenges of DER systems

Distribution systems become more complex with the interconnection of distributed energy resources (DER) and the addition of power electronics and controls. Eaton’s CYME software applications support the advanced simulation of the entire network, to allow detailed and reliable modelling.

Design and modelling

Network Editor

The Network Editor features a user-customisable graphical user interface underlying the CYMDIST applications and the complementary CYME analyses modules.

This includes extensive modelling capability of distributed energy resources (DER) equipment and energy storage; along with the definition of all customer types necessary. The software also includes control models that are relevant to the various generation sources. All libraries can be enriched by users.

The Network Editor is included in the Distribution System Analysis package (CYMDIST).

Enhanced substation modelling

This module enables the accurate representation of all the major components of a distribution substation, as well as  any sub-network, such as a vault, a switching cubicle or an industrial facility. The simulations then take into account the effects of these installations on the overall distribution system.

Low-voltage secondary distribution modelling


The low-voltage secondary distribution model performs the detailed modelling and simulation of any circuit beyond the distribution transformer. This includes single-phase centre-tapped transformers, plex cables, single-phase three-wire LV circuits.

Secondary grid network analysis

Secondary grid network analysis allows users to model any spot network, secondary grid and detailed network protector relay with complete settings. The module is equipped with robust power flow and short-circuit algorithms to analyse heavily meshed networks.

Online maps service

Display Google Maps and MapQuest Open maps as layers underneath the geographical view of your electrical network model. With this service, users can locate a substation, a particular feeder, a street corner, or pinpoint the address where a fault occurred.

Geographic overlay


Geographic overlay displays raster or vector map images (geographical landbase such as DWG, DXF, SHP, etc.) as layers directly underneath your electrical model. The module allows the import and display of several maps in different formats, so your users can visualise the distribution system over a comprehensive landbase.

Power system analysis

Distribution state estimator

Process various measurements to estimate the load and power flow as well as the voltages of the system based on any type of electrical model to determine the best solution. The analysis solves for radial, looped and meshed networks.

Dynamic data pull

Refine the as-built planning model with field measurements such as power, current, voltage, load demand, generation or device statuses for switches, voltage regulators and shunt capacitor banks.

Advanced fault locator

Reports all the possible fault locations, taking into account multiple monitoring elements, fault indicator statuses and monitored data from COMTRADE files.

Distributed energy resources

Integration capacity analysis

Integration capacity analysis addresses the interconnection requests by calculating the maximum generation or load capacity that can be installed independently at each point of a distribution system without adversely affecting its reliability and power quality.

EPRI DRIVE

Seamlessly integrated into the CYME software graphical user interface, the EPRI DRIVE module combines the engineering effort of the EPRI DRIVE engine with CYME’s detailed distribution system model to return hosting capacity calculation results within a familiar environment.

DER impact evaluation

Generation interconnection system impact studies can be executed within minutes with this module. It clearly assesses the impacts of DER interconnections on the distribution system, such as steady-state voltage levels, overloads and reverse power flow. The module executes a comprehensive system impact study that integrates several criteria-based verifications and multiple scenarios in order to flag abnormal conditions.

Network disturbance assessment

The network disturbance assessment module evaluates the power quality disturbances produced by equipment on a power source’s signal, by determining if the equipment passes different power quality tests. Analysis is based on the standard “Technical Rules for the Assessment of Network Disturbance” published by a German-Austrian-Swiss-Czech working group.

Long-term dynamics load flow analysis

This module performs time series long-term dynamics load-flow analysis in the seconds to minutes range, of the variable phenomena introduced by distributed energy resources. Device controls are included in the analysis, including tap changers, shunt capacitors and switchable shunt banks. It also enables the time-domain simulation of smart inverters and battery energy storage systems.

Distribution automation

Reliability assessment module

The module computes reliability indices for the overall system and corresponding protection zones, as well as customer point indices. The predictive model can be calibrated based on historical data. The user can analyse different system configurations and measure the improvement in reliability indices.

Optimal re-closer placement

Working with the Reliability Assessment module, it takes into account objectives and criteria, studies the reliability indices, and evaluates the expected improvement to find the optimal locations for re-closers.

Contingency assessment and restoration

This module is a comprehensive tool for studying the impact of contingencies on the distribution system. It supports assessment of the robustness of the networks by identifying potential problems with outages and planning maintenance, and finding an optimal switching plan for power restoration

Volt/VAR optimisation

Identify the optimal configuration of installed capacitors, the inline regulator and the LTC transformers in a distribution system. The calculations take into account constraints on the network as well as objectives such as peak shaving, reduced system losses and improved voltage profile, in order to optimise system efficiency.

Optimal voltage regulator placement

Use this module to determine the optimal location and set the tap position of voltage regulators, as well as determine the amount of regulators needed to achieve the desired voltage regulation.

Protective device analysis

This module helps power engineers effectively address protection issues by analysing time-current curves. The library contains over 15,000 protective device curves.

Module features: network protection analysis, minimum fault analysis and sequence of operation.

Time-series analysis

Long-term dynamics load flow analysis

This module performs a time series long-term dynamics load flow analysis  of the variable phenomena introduced by distributed energy resources, in the seconds to minutes range. Device controls are included in the analysis, including tap changers, shunt capacitors and switchable shunt banks. It also enables the time-domain simulation of smart inverters and battery energy storage systems.

Steady state analysis with load profiles

This module executes time-series load-flow analysis based on the profiles modelled from a combination of historical consumption patterns and real-time monitoring data, such as SCADA, AMI, MDM, AMR, etc.

ENTERPRISE INTEGRATION AND AUTOMATION SOLUTIONS

CYME GATEWAY

Extract all necessary information from your GIS and other enterprise systems to automatically generate up-to-date and accurate distribution network models, ready for planning and operational studies executed with the CYME software.

CYME Server

This module enables a large number of users to simultaneously and concurrently perform CYME simulation requests from various client applications; DMS, OMS, EMS, SCADA, GIS, etc.

Low-voltage secondary distribution modelling

Refine the as-built planning model with field measurements such as power, current, voltage, load demand, generation or device statuses for switches, voltage regulators and shunt capacitor banks.

Data push publishing

This is a customised bridge built between the CYME software and the external systems desired, based on the extensive CYME keyword library.

X
Download Close

Contact me

Ved at indsende denne formular accepterer jeg, at de personlige data, som jeg giver, kan deles med Eaton, kanalpartnere og tredjepartsudbydere på vegne af Eaton i overensstemmelse med Eatons privatlivspolitik og i overensstemmelse med gældende databeskyttelseslovgivning.
Jeg accepterer, at Eaton regelmæssigt informerer mig om deres produkter, kampagner og nyheder. Jeg forstår og accepterer, at Eaton vil bruge mine data, inklusive adfærdsmæssige data såsom visninger af hjemmesider og videoengagement, for at målrette markedsføringskommunikation. Jeg forstår, at jeg til enhver tid kan trække mit samtykke til at modtage markedsføringsmateriale tilbage.