Leveraging selectivity to deliver overcurrent protection and critical load power availability
While safety through circuit protection is always the first priority, there are scenarios – especially in large, low-voltage installations – where total power shutdown while a localised problem is resolved would deny power to critical loads elsewhere. Learn how selectivity safely isolates faults but keeps critical loads up and running.
Author: Sebastian Oberwelland, Commercial & Industrial Buildings Segment Leader, Electrical Sector, EMEA
The basic premise of selectivity (previously known as ‘discrimination’) is simple. It is the coordination of overcurrent or residual current protection devices in serial connection, so that a fault in the installation is cleared by the protection device located immediately upstream of the fault. Overload protection devices such as fuses, different types of circuit breakers or residual current devices prevent unwanted tripping and` preserve system availability. The aim is to limit the number of loads that will be disconnected from the power supply if a fuse or breaker trips. So where and how best should selectivity be used?
International standards state that harnessing selectivity is a highly recommended, rather than mandatory, approach. And it’s one that offers particular benefits when it comes to electrical installations in marine applications and high-rise buildings, as well as systems where reliable power is crucial, such as those supplying medical devices, data centres or any other type of critical infrastructure. Further examples of the latter include life safety equipment such as sprinklers, smoke extractors, fire pumps and lifts that need to continue operating no matter the possible damage due to overcurrent.
Selectivity of two protective devices can be total, partial or none. Total selectivity is achieved where the overcurrent protection device on the load side will operate up to the maximum prospective short circuit current at its point of installation. In case of partial selectivity, the overcurrent protection device on the load side will operate up to the fault current, which is less than the maximum prospective short circuit current at its point of installation. This is expressed by selectivity limit current (Is).
While this division is accurate, from a practical point of view we’re ultimately interested in whether the combination of protective devices used in a given location is selective or not.
Various methods to ensure selectivity include:
Time-current selectivity takes both factors into account to solve selectivity under all expected circumstances.
Most of Eaton’s electronic trip units, such as those used in our air circuit breakers (IZMX/NRX) and moulded case circuit breakers (digital NZM series), offer this smart feature. Even better, communication between our devices with ZSI does not require an external power supply or any external modules.
The introduction of our latest NZM circuit breakers now brings further improved selectivity capabilities. These models – available from 2024 starting with NZM frame size 3, followed by frame size 2 – significantly improve overall system design. When a NZM3 breaker is used upstream with an NZM2 downstream, total selectivity is achieved, enabling smarter switchgear than ever before.