Download document () of 20
  • Streamlining design efficiency

Best practices to optimize design and construction schedules, budgets

In an industry where the pace of construction is only accelerating and project timelines are compressing, consulting-specifying engineers are being asked to deliver more – faster. But with productivity in global construction declining by 8% from 2020 to 2022, backlogs are already straining teams. How do we design and build smarter without cutting corners?

According to McKinsey research, the construction industry could grow by 70% by 2050. That growth brings opportunity and significant pressure. Many engineers and consultants are already struggling to keep up with today’s demand. Improving the tools used to design and specify electrical systems presents a powerful opportunity to drive productivity, reduce delays and control costs.

CIBSE, the Chartered Institute of Building Services Engineers, is a trusted voice in building construction. Their continued focus on adaptations towards net zero, and energy efficient buildings has highlighted the need for advancements in engineers’ tools; maximizing output and therefore widescale rollout of digital and sustainable enhancements.

The message is clear: improved and better integrated tools, proactive collaboration, and more flexible approaches to design are essential to keeping projects on track.

Collaborative expertise is critical to accelerate projects

In today’s fast-paced construction environments, efficiency begins with early and proactive collaboration. Engaging manufacturer application engineers (AEs) from the start helps streamline the design process, reduce rework and keep projects on schedule.

AEs bring deep technical insight and practical application knowledge to the table. Engaging them during the conceptual phase – when ideas are still rough sketches and/or your client’s scope is not fully clear – ensures better system compatibility, eliminates guesswork, and provides early layouts and budget estimates that can help guide design decisions in the right direction.

Eaton Two engineers looking at blueprints

From there, collaborative development of submittals and bills of material avoids redundant reviews and miscommunications. At Eaton, we work side-by-side with consultants through live collaboration platforms to finalize submittals quickly. We also leverage artificial intelligence (AI) internally to boost productivity, using tools that analyze drawings and specifications, flag exceptions and automate configurations. Combined, these collaborative and digital design capabilities can help reduce project timelines by 4 to 6 weeks or more.

Further, our AEs are trained to support smarter project sequencing. For instance, if only two of 20 switchboards are needed early to energize a site, identifying those priorities allows us to fast-track delivery and strategically tap regional manufacturing facilities to secure priority production slots. In these times of unprecedented demand, these strategic insights help consultants add value to keep construction moving, even amid tight schedules and supply chain constraints.

Eaton AEs can also help you take advantage of the latest digital tools that simplify system design, specification and reduce duplicated efforts. From providing drawings in native computer-aided design (CAD) and building information modeling (BIM) formats to fully edited product specifications, let’s look at how these tools are changing the way projects get done.

Three key tools helping streamline the design and specification process

Modern tools are changing the game for how consultants design, specify and manage electrical systems. Here’s how: 

1. Instant specification, pricing and BIM integration

Eaton’s internal BidManager tool is a powerful resource our AEs use to support complex project needs. This tool generates comprehensive technical packages, including accurate BIM files, CAD drawings, pricing estimates and bill of materials (BOMs) for both standard and custom-configured solutions. The tool even provides our AEs with expected manufacturing lead times based on the specific configuration, which can be especially impactful during the planning phase.

Eaton’s expansive product portfolio combined with our AEs deep domain expertise ensure all available product options and distribution approaches are considered to find optimal solutions. BidManager’s drawing and digital configuration outputs are generated based on your project’s specific requirements to make sure all relevant technical design details are included – such as adequate space needed to safely install and maintain equipment.

Additionally, through our integration with Autodesk Revit, the files generated by BidManager provide engineers with confidence that every configuration is dimensionally accurate and fully manufacturable from the outset. It also helps reduce the need for manual data entry and helps prevent costly errors later in the process. 

eaton-buildings-as-grid-simulator-desktop.png

2. Buildings as a Grid simulator

Eaton’s proprietary Buildings as a Grid Simulator empowers building managers and consultants to make informed decisions and invest in electrical infrastructure that aligns with the project’s goals whether this is energy efficiency, cost savings, sustainability, or a combination of these.

The tool helps design an approach that fits the unique usage patterns of the site. Using the simulator, Eaton engineers can calculate and advise on the optimal investment and technology upgrades while also determining the financial outcomes, enabling you to make effective data-driven decisions. By evaluating energy load profiles, grid connection potential, local renewable energy sources, and energy storage options, the data-driven results enable stakeholders - including investors, operators, occupants, and facility managers—to maximize their building's potential.

3. Switchboard design support

Low voltage switchboards play a decisive role in supplying electrical power. Demands placed upon these switchboards, particularly as operations and infrastructures expand over time, leave them vulnerable to arc flashes. Eaton offers a comprehensive range of solutions to help reduce the risk of injury and costly damage caused by an arc flash.

One key material, The Consulting Application Guide, Low Voltage Volume is designed to assist electrical consultants, electricians or power system design engineers in the layout and specification of equipment.

This Consulting Application Guide has been drawn up by a group of experienced experts, with respect to standards for electrical installations (IEC 60364 series) and other product standards. This edition contains many products, services and application-specific information.

NTI Experience Center feature block

Comprehensive education and specification solutions make your job easier    

Digital design and specification innovations are only as powerful as the people using them. That’s why Eaton invests in a wide variety of educational content including in-person and hands-on training.

Additionally, Eaton offers a complete range of on-demand and remote educational solutions that enable electrical professionals to stay up to date on the latest industry best practices as their own schedule dictates.  Eaton’s local experts can also provide continuous professional development (CPD) courses that can be held at a customer or consultant site.  

 

 

Main CPD topics include:   

  • Arc flash in switchboards
  • Low voltage switchgear
  • Arc fault detection devices
  • Principles of emergency lighting design
  • PAVA (public address and voice alarms)
  • Energy storage systems
  • Commercial scale EV charging

Further, our consultants portal provides power system designers with a comprehensive collection of design tools, educational resources, product information and other helpful documentation. Traditional catalogs offer part numbers and static data, but our design tools go a step further, helping consultants answer not just what to use, but whywhen and how to use it. 

For instance, our design guides can help users identify the correct product configuration for the job based on technical requirements such as cable entry, ratings, heat dissipation and applicable code requirements. From there, you can easily pull the correct BIM file and generate product specifying guides to help save time creating files and avoid writing specs from scratch.

Simplify upfront electrical system design to accelerate entire projects

The construction industry is evolving rapidly, but the pressure to deliver on time and on budget isn't going away. Tackling complexity at the front end through collaboration and smarter tools can dramatically improve project outcomes.

By working closely with manufacturers like Eaton, engaging application engineers early and leveraging advanced digital tools, consulting-specifying engineers can:

  • Simplify and accelerate the design process
  • Avoid costly revisions and change orders
  • Compress the timeline from planning to product delivery

At Eaton, our people, tools and platforms are designed to support this shift toward faster, smarter projects. Whether you're designing a hospital, data center, or commercial campus, we're here to help you cross the finish line with fewer delays and greater confidence.

Let’s simplify the building lifecycle—together.
Reach out to your local application engineer to get started and visit our consultants portal to learn more.

Additional resources