How to create interfaces that are intuitive to use
Actions, terminology and commands should be presented – and behave – consistently from use to use. Repeatability helps the user learn faster and find information more quickly. Design elements such as icons, buttons and navigation menus must also be consistent.
Intuitive and user-friendly controls can only be designed when you have a grasp of the precise data users need to read and enter in the HMI interface to minimize complexity.
To achieve simplicity and clarity when designing HMI interfaces, on-screen buttons have an important role to play. So maximise their potential for helping the user to easily navigate the touch screen panel.
A GUI’s color theme must reflect your organization’s corporate identity. Light and dark themes can be used, depending on the operating environment’s lighting scheme.