Download document () of 20
Fire detection systems

Conventional EN & UL reflective beam detector

Eaton's advanced beam detector, EF-CBD50, is for use with the Eaton range of conventional fire systems. It prioritises ease of installation, whilst incorporating substantial performance improvements over previous models. This detector has been re-designed to remove the need for specialist tools or knowledge for installation and operation. One person can install the product and initiate the auto-alignment procedure for hassle free commissioning.

There are two versions of the detector, differentiated by either EN54 or UL certification. Each baseline model has a range of up to 50 metres. This can be extended to 120 metres with the additional long range kit.
Intuitive
One person installation and commissioning
Efficient
Cost-effective smoke detection for large, open areas
Adaptive
Adapts to installation environment

Reflective beam technology: How does it work?

A beam smoke detector works by sending, an invisible infra-red (IR) beam of light across the protected area, to a receiver. The receiver measures the strength of the beam. If smoke is present in the air this obscures, or decreases, the light received. When enough smoke is in the air the IR light level will drop below a set threshold, which then triggers an alarm condition. 

EF-CBD50 uses the reflective method. This means that the IR transmitter and receiver are housed in the same unit. A reflector is placed at the opposite end of the protected area to the detector. The reflector bounces the light beam back to the detector for processing. This is a widely used method that offers reduced installation cost and time, compared to having the transmitter and receiver as separate units.

fire-conventional-how-a-reflective-detector-works-infographic.jpg

One person installation and commissioning

The beam detector incorporates a bank of buttons conveniently placed on the front of the unit. The area also includes LEDs that clearly indicate the operational status of the device. This means product setup and further adjustments can be carried out intuitively, without the need to remove the product from the installation point.

Once the hardware has been installed, the detector buttons can be used to steer a targeting laser onto the reflector. Auto-alignment can then be initiated with the press of a button. In addition, the required detection sensitivity can also be set using the settings switches.

fire-conventional-reflective-detector-install-infographic-1.jpg
  1. Alignment status indicators
  2. Slide switch
  3. Direction settings
  4. Settings switch

A beam detector that can adapt to its surroundings

Not only does the EN and UL certified reflective beam detector have dynamic beam phasing that prevents interference between detectors that face each other, or others that are in irregular configurations, it can also adapt to environmental changes.

fire-factory-icon-blue.png

Building movement

When installed correctly, the detector can adjust its own alignment to compensate for natural building movement over time.

fire-bulb-icon-blue-1.png

Changes in lighting

Light cancellation technology compensates for high levels of sunlight and artificial lighting, that would otherwise cause nuisance alarms. 

 

fire-truck-icon-blue.png

Dirt and dust build-up

In dusty or dirty environments, the detector can compensate for gradual build-up of contamination that would interfere with the IR beam. 

Cost-effective smoke detection for large, open areas

The EN & UL certified beam detector replaces the need for large quantities of individual point detectors in large open areas such as commercial warehouses, airports, schools and arenas. A building with a large area may require up to 52 point detectors to ensure safe coverage, whereas two beam detectors could provide coverage of the same area. This helps deliver a more practical and cost effective solution, whilst making system installation, commissioning and testing much simpler.

Efficiency in power and connectivity

The detector consumes just 5mA in all standard operational modes. It will align itself in under a minute if Fast Alignment is selected. In this mode, the current consumption will increase to 33mA and then revert back to 5mA once aligned. If Fast Alignment is off, the unit will draw 5mA current, but will take up to 15 minutes to align itself. If these current requirements are factored into the system design, the product can be used on Eaton conventional zone without the need for an additional power supply unit. Fire and fault conditions are signalled to the panel using standard zone wiring, so no additional interconnections are required.

Project perfect, view our range of conventional fire alarm devices

Specifications

Highlight differences
Show only differences
Hide blank features

Technical specifications

Detection performance
Detection range

0 to 50m

0 to 120m with Reflective Long Range K

Alignment method Laser assisted, Auto-Alignment™. Manual alignment – optional setting
Auto-Alignment™ protocol Background check, Box search, Adjust and Centre
Building Movement Tracking™ Compensates for natural shifts in alignment from building movement*
Contamination Compensation Compensates for gradual build-up of contamination on the optical surfaces
Light Cancellation Technology™ Compensates for high levels of sunlight and artificial lighting
Optical wavelength – smoke detection 850nm near infrared (invisible)
Integrated laser – laser alignment 650nm visible. Class IIIa <5mW
Dynamic Beam Phasing

Allows beam detectors to be mounted facing each other with the reflectors in the middle.

Eliminates false alarms caused by crosstalk between beams

Signal output Individual Alarm and Fault relays (VFCO) 2A @ 30 VDC
 
Programmable user settings
Alarm response threshold levels

25% (1.25dB) – Fastest response to smoke

35% (1.87dB) – Default value

55% (3.46dB) – High immunity to false alarms, slow response to smoke

85% (8.23dB) – Highest immunity to false alarms, slowest response to smoke

Configured via the integrated user interface

Delay to Alarm 10 seconds, for momentary partial obstruction of the beam path
Delay to Fault 10 seconds, for momentary obstruction of the beam path
 
User features
Integrated user interface Alignment mode switch, alignment directional buttons and configuration switches for alarm response threshold
Alignment status indication 2 Green LEDs and 1 Yellow LED
System status indication

Normal operation – Green LED flashing every 10 seconds

Alarm condition – Red LED flashing every 10 seconds

Fault condition – Yellow LED flashing every 10 seconds for obscuration or every 5 seconds for contamination

Flat front face with enclosed optics. Cleaning the optics does not affect alignment

 
Design parameters
Separation distance between Detector and Reflector

5 to 50m

50 to 120m with Reflective Long Range Kit

Beam path clearance 1m in diameter from centre line between Detector and Reflector
Detector dimensions Width 130mm x Height 181mm x Depth 134mm (see diagram)
Reflector dimensions

Up to 50m separation distance – Single reflector 100mm x 100mm x 9mm

Up to 120m separation distance – Four reflectors arranged in a square pattern 200mm x 200mm x 9mm

Product weight Detector – 0.7kg; Reflector – 0.1
Multi-detector arrangement Dynamic Beam Phasing allows for Detectors to face each other with the reflectors in the middle
Housing colour White RAL9016, UV stable
 
Electrical specifications
Operating voltage 14 to 36 VDC
Operating current (constant) all operational modes All operational modes – 5mA; Fast alignment mode – 33mA
 
Field wiring
Cable gauge and type

2 core, dedicated, 0.5 to 1.6mm (24 to 14 AWG)

System compatible with fireproof and non-fireproof cable meeting local installation standards

Cable entry

3 knock-out locations capable of accepting M20, ½” or ¾” glands

4 drill-out locations capable of accepting glands up to 21mm diameter

 
Test and maintenance
Alarm test Optical alarm test using Commissioning and Maintenance Kit accessory
 
Environmental specifications
Operating temperature -20 to +55°C
Storage temperature -40 to +85°C
Relative humidity (non-condensing or icing) 0 to 93%
IP rating IP55
Housing flammability rating UL94 V0 polycarbonate
NB: All figures are quoted for 25°C
 
Optical specifications
Fault level / Rapid obscuration (Δ ≤ 2 seconds) ≥85%
Maximum angular alignment of Reflective Detector ±4.5° (±70° with adjustment bracket accessory)
Maximum angular misalignment of Reflective Detector ±0.5°
Maximum angular misalignment of Reflector ±5°
*When mounted according to manufacturers guidelines
Download Links
X
Download Close
Looking for Cooper, JSB or Menvier?