Download document () of 20

Eaton E-series protective relays:

Troubleshooting parameter settings

View all of Eaton's protective relays

Troubleshooting parameter settings

Problem or maloperation in…

Problem description

Corrective action

Transfer of device parameters from one protection device to another of the same type (e.g. EDR-5000). You have configured the parameters of a ESeries device. Now you want to transfer these parameters to another relay. This is possible, if both relays are of the same type, e.g. EDR-5000.

Download the device parameters with PowerPort-E from the first relay. Save them into a file.

Now reopen this file with PowerPort-E. Adapt the settings to the order code of the second device <Edit/Modify Device Configuration (Typecode)...>. Select <Apply>. By this the existing parameter file is being converted to the format of the second device.

Now there may be implausible parameters. They are marked with a question mark. These are not valid for this device type. Please adapt the values of these implausible parameters. Afterward you can transfer the parameter settings to the second device.

Go back to the main troubleshooting protective relays page.

 

For additional support

For additional manufacturer technical support, please contact 1-800-809-2772, option 4, then option 1 or use the email address, MRsupport@eaton.com.