Download document () of 20

Eaton E-series protective relays:
Troubleshooting the event recorder

View all of Eaton's protective relays

Troubleshooting the event recorder

Problem or maloperation in…

Problem description

Corrective action

The Event Recorder is permanently logging new events.

The Event Recorder does permanently show new events (<Operation/ Recorders / Event rec>).

To observe this phenomenon in PowerPort- E, please execute a "refresh" (F5 or Ctrl+F5).

Proceed as follows:

  1. Look inside the Event Recorder which protection function is creating the events.
  2. Check the settings of this protection function. Adapt them, if necessary. Example: Protection function df/dt (ROCOF) is configured too sensitive and is creating alarms with high frequency. Change the settings of this function.
The Waveform Recorder is permanently creating new records.

The Waveform Recorder shows a high number of created disturbance records. This number is growing steadily over time (<Operation/ Recorders / Waveform rec>).

To observe this phenomenon in PowerPort-E, please execute a "refresh" (F5 or Ctrl+F5).

Check the following issues:

  1. Check which events are configured to trigger the Waveform Recorder (<Device Para/ Recorders / Waveform rec>), e.g. Protection Alarm.
  2. Check within the Event Recorder, which protection function creates the trigger (<Operation/ Recorders / Event rec>).
  3. Check the settings of this protection function. Adapt them, if necessary. Example: Protection function df/dt (ROCOF) is configured too sensitive and is creating alarms with high frequency. Change the settings of this function. Alternatively you can also change the trigger source of the Waveform Recorder. But this is less advisable.

Go back to the main troubleshooting protective relays page.

 

For additional support

For additional manufacturer technical support, please contact 1-800-809-2772, option 4, then option 1 or use the email address, MRsupport@eaton.com.