Download document () of 20

Troubleshooting Eaton E-series protective relays:

Self-supervision Error Codes

The protection device supervises its normal operation by executing various self-supervision checks during runtime of the device.

When detecting any serious faults, the system LED will start flashing alternating red and green. The issue will be recorded in an internal memory.

Please check the self-supervision error code under <Operation/ Self Supervision/ System Error>.

View all of Eaton's protective relays

Troubleshooting Self-supervision error codes

Self-supervision Error Code, last failure

Message Description

Corrective Action

1 The device suffered an unscheduled restart.

Get in contact with our service-team.

You will be supplied with a tool for error analysis.

2 - 4 Critical level of internal resources.

Get in contact with our service-team.

You will be supplied with a tool for error analysis.

5 - 10 reserved for future use.  
11 Hardware: FRAM defect. The device will be set out-of-service on next reboot. Send the device for repair.
12 The battery for buffering the real time clock is low. The battery can be exchanged by the manufacturer. There's no impact on the functionality of the device if the battery breaks down, except for the buffering of the clock while the unit is in deenergized condition.
13 reserved for future use.  
14 Your device suffered a short-term sag or outage of the supply voltage. Please check your power supply. You can quit the System LED by selecting <Operation/ Reset/ SSV.Ack System LED>.
15 Critical level of internal resources.

Get in contact with our service-team.

You will be supplied with a tool for error analysis.

16 - 35 reserved for future use.  

Go back to the main troubleshooting protective relays page.

 

For additional support

For additional manufacturer technical support, please contact 1-800-809-2772, option 4, then option 1 or use the email address, MRsupport@eaton.com.

NOTE: You can find the Error Code under <Operation/ Self Supervision/ System Error>

For additional support

For additional manufacturer technical support, please contact 1-800-809-2772, option 4, option 1, or pqsupport@eaton.com.