MyEatonFAQs
Cables crossings module
When two cables cross each other, each behaves as a heat source for the other one. The amount of generated heat, the vertical distance between the crossing cables and the crossing angle are the main parameters influencing the crossing rating.
In the absence of crossing calculations, the general practice is to use the conservative result where the circuits are assumed to be parallel. When cables are parallel, the thermal interaction is maximum. The conservative approach unnecessarily de-rates both cables.
With the cables crossing module, users can achieve ratings up to 20% higher than the conservative ampacities obtained based on the parallel installation scenario.
Cable impedance calculation module
Magnetic fields module
Short circuit cable rating module
Duct back optimizer module
Parametric studies module
Soil dry-out analysis module
Multiple duct banks and backfills module
Advanced tunnel modeling module
Cables in troughs module
Submarine cable installations module
3D modeling module
We are committed to delivering best-in-class solutions and providing exceptionally focused customer service. Our dedicated experts work closely with engineers throughout the entire project to successful completion.