Download document () of 20
We make what matters work*
  • Parametric studies module

    The parametric studies module (CYMCAP/PARAM) allows cable engineers to perform simulations in batch mode by varying one or more installation parameters.
    Contact me about this module

Streamline cable ampacity simulations with unlimited variable parameters

The parametric studies module is a powerful tool that assists cable engineers in performing batch-mode simulations. Rather than utilizing fixed specific parameters, users can define a range of values for multiple selected parameters, including soil temperature, soil resistivity, installation depth, distance between cables and installation dimensions. This module allows users to save time and produce more meaningful results. 
parametric-studies.jpg

Highlighted features 

  • Analyze and review the relation among various parameters and the thermal/current rating of cables through graphics and reports
  • Determine the effect of user-defined parameters in the simulation
  • Design with a flexible tool that supports an unlimited number of variable parameters
  • Create automatically selected executions corresponding to a specific simulation
  • Develop a summary report containing the main results for relevant cases

Ready to learn more about this module? 

engineer looking at computer

Do you have questions about this module?

We are committed to delivering best-in-class solutions and providing exceptionally focused customer service. Our dedicated experts work closely with engineers throughout the entire project to successful completion.