The unfilled troughs module offers four approaches for finding ampacity in unfilled (air-filled) troughs: the IEC standard, Slaninka method 1, Slaninka method 2 and the Anders coates method. These approaches are based on field research conducted by independent parties and published in scientific journals. Depending on the selected method, users can enable additional factors that might influence the thermal behavior of the installation, such as the native soil thermal resistivity, the trough's cover material and the wind velocity over the trough.
Filled troughs are supported by the multiple duct banks and backfills module. The ampacity (or operating temperature) is computed using the IEC standardized method, except for the external thermal resistance T4, which requires a finite elements approach.
We are committed to delivering best-in-class solutions and providing exceptionally focused customer service. Our dedicated experts work closely with engineers throughout the entire project to successful completion.