Télécharger le document () de 20
Nous agissons afin que ce qui compte fonctionne*

Integrating functional safety in machines and systems

Safety manual for machines acording to EN ISO 13849-1 and IEC 62061
 
SISTEMA,  VDMA 66413 product data, safety characteristics
 
Updates on Machinery Directive, EN ISO 13849-1 and EN IEC 62061
 
Download white paper

Switch off and work safely

Functional safety is an essential part of the design process for machines because it is key to protecting the wellbeing of the machine operator and keeping production up and running. To ensure functional safety, the latest guidelines have to be applied - design guidelines with standardized and accepted circuits can help to notably reduce implementation efforts.

For more than ten years, DIN EN 60204-1 has ensured the safe design of electrical equipment for machines and plants. The underlying IEC 60204-1 standard was updated in 2016 - now the European version of the world's most widely used machine safety standard is published. This whitepaper provides an overview of the most important changes for machine and plant manufacturers, especially with regards to switchgear technology.

 

functional-safety-switch-inuse
eaton-functional-safety-eu-directives-and-standards-graphic-en-us.jpg

Internationally harmonized regulations, known as EU Directives, are in place to ensure balanced protections for people and the environment and to reduce competitive disadvantages and hurdles to business due to different safety regulations within the EU. 

The safety of machines is primarily covered within two directives. The Machinery Safety Directive is oriented toward producers of machines, while the Work Equipment Directive is oriented toward operators of machines. A principle known as the 'Presumption of Conformity' applies to the fulfillment of requirements defined in harmonized standards. It presumes that the protective goals of the EU directive are to be regarded as sufficiently met.

Our safety manual gives you an overview of the most important directives, standards and regulations for machines in the EU.

Updates on Machinery Directive, EN ISO 13849-1 and EN IEC 62061

The Change of the Machinery Directive 2006/42/EC to the Machinery Regulations as well as the update EN ISO 13849-1 and EN IEC 61061 in 2021 and 2022 and how this effect machine and system builder are described in the white paper.
question mark blue white

Frequently Asked Questions

What is functional safety of machines and how can it be increased

What are the eight most significant changes to EN 60204-1?

The machinery regulation replaces machinery directive 2006/42/EC. What is changing? 

Machine safety: How does a risk assessment work?

What does the CE marking on a machine tell us?

Which standards must be followed for machine safety?

Emergency stop vs. emergency switching off: what's the difference?

Why were the standards EN ISO 13849 and IEC 62061 revised in 2021, and how do these updates affect engineers’ work?

 
Didn't find what you are looking for? Find here more answers to machine building topics.

Find out how you can control the unexpected in our safety manual

Safety manual

The Eaton Safety Manual provides an easy entry-level into the extensive set of material available on safety technology. The manual contains an overview of the most important factors of directives, standards and regulations that have to be taken into consideration when using safety equipment on machines.
question mark blue white

Frequently Asked Questions

How is the safety integrity level determined in accordance with IEC 62061? 

How do you determine the performance level in accordance with EN ISO 13849-1?

How do Performance Level (PL) and Safety Integrity Level (SIL) differ?

What does the circuit diagram for a two-hand control look like?

How to design an emergency stop circuit for an e-stop switch?

How can movable guards such as protective doors on machines be reliably monitored?

How can open hazardous areas be monitored using light curtains as a protective device?

What does safe motion mean and how do STO and SS1 safety circuits look like?

Didn't find what you are looking for? Find here more answers to machine building topics.

Implementing functionally safe circuits with the right products

Emergency stop push buttons for various applications
Emergency stop push buttons for various applications
Emergency stop pushbutton RMQ compact Series  with cable and M12 plug
Emergency stop pushbutton RMQ Compact Series with cable and M12 plug
Safety contactors with non detachable auxilary switch identified by yellow cover
Safety contactors with non detachable auxilary switch identified by yellow cover
Safety logic, safety relay, safety logic relay
Safety logic like safety relay and safety logic relay
Safety positioning switches and safe non contact switches
Safety positioning switches and safe non contact switches
eaton rotary cam switches shafts handles accessories
Switch disconnectors
Horizontal photo rear back businessman sitting at desk points on laptop screen empty mock up copyspace analyse market company development. Internship mentoring concept banner for website header design