Ladda ner dokument () av 20

Feeder Automation Manager software

Eaton’s Yukon Feeder Automation (YFA) solution is an advanced feeder automation software that focuses on self-healing grid functions such as FLISR (Fault Location, Isolation, Service Restoration). The system is designed to help lower SAIDI and SAIFI metrics by converting sustained outages into momentary outages by means of automated intelligent switching operations. The YFA system leverages real-time data from Intelligent Electronic Devices (IEDs) on the distribution system, to detect system disturbances such as faults and then automatically reconfigure the system to isolate the disturbance and minimize the total number of customers impacted by an outage. Eaton’s Yukon Feeder Automation solution provides utility engineers with the tools to easily design and implement a self-healing grid solution. The YFA system makes changing the automation settings effortless, thereby streamlining the process of incorporating new IEDs or adapting to changing field conditions. The YFA system ease-of-use empowers utilities to incorporate the self-healing grid as a process rather than treating feeder automation as a project.    

Leverage real-time data
Improved reliability
Dynamic self-healing software
Minimize customer impact
Reduce SAIDI/SAIFI
Better system metrics

Viktiga egenskaper

  • Fault management, voltage loss management and load management
  • Simple configuration
  • Self-healing system
  • Server-based application with centralized communication architecture

Faster restoration for better system performance

Performs service restorations in approximately 30 seconds to 2 minutes, significantly reducing outage time, SAIDI and SAIFI.
Specifikationer

Yukon Feeder Automation (YFA) features

FAULT MANAGEMENT

Quickly detects and isolates faults so that unaffected load sections can be restored via feeders with capacity

VOLTAGE MANAGEMENT

Detects loss of voltage situations and can isolate those line sections from the feeder, so that the unaffected sections can be restored

LOAD MANAGEMENT

Continuously monitors loading on the system to help prevent overload in the case of an event

DISTRIBUTED ENERGY RESOURCE INTEGRATION

Allows for the integration of Distributed Energy Resources on the system and understands by directional-current flow

Can even help to control those resources and manage which feeders to which they are connected

MULTIPLE OPEN PROTOCOLS

Automation System is not locked into a proprietary format

FLEXIBLE COMMUNICATIONS

The system can leverage existing communication networks without the need to establish a new or separate network for automation 

EASY DEVICE INTEGRATION

Controls from many different manufacturers are available via pull-down menus to integrate those devices easily in the system. This feature means that YFA software does not lock the utility into a single vendor. We also add new devices to the system upon request so that the automation system is future-proof as new devices are developed.

DYNAMIC TOPOLOGIES

Does not need to be in a "normal" topology to function correctly;  this means YFA software can respond in many different situations for a number of different faults

SIMPLE CONFIGURATION

Makes setting up the YFA system straightforward and allows utilities to truly own their automation system

MINIMAL LINEMAN AND OPERATOR TRAINING

A fully automatic restoration system that requires very little interaction with operators

Is adaptable to the utility's current work practices and can be disabled via in the field commands such as hot line tag or local mode or via operator commands

BUILT-IN SIMULATOR

The exact same logic that powers the automation engine on a YFA simulation machine also powers the YFA production machine

Testing done in simulation can accurately reflect how the production system will operate

This is very different from distributed systems where a simulator can only approximate what might happen because each device\agent operates semi-independently on those types of system and the simulator always runs on a PC, not the actual hardware

SCALABLE

Can be deployed to control a system as small as two devices and has operated on systems over 800 feeders in size

The simple configuration makes YFA both very scalable, but also easily maintainable  as the utility infrastructure evolves

CENTRALIZED AUTOMATION TRACE

Since all of the data for a YFA system  comes to a centralized location, it is all logged, timestamped and stored in that one location

This makes understanding what happened easy with human readable log events and reports

This allows for a system of continuous improvement on the automation system so that it can be optimized to operate exactly how the utility wants it to be

OPTIONAL REDUNDANCY

YFA has the option of having a fully redundant hot standby system, so that if something were to happen to the primary machine, the secondary machine could fill in and take over the system

SECURITY

YFA has undergone extensive security testing and assessments to ensure that it is compliant with the latest best practices in cybersecurity

YFA uses Windows Active Directory for Authentication and ties in roles specific authorization based on that authentication

This allows different users and groups to access the system, but only allows those with the right privileges to  make modifications

All of the modifications are tracked and recorded

Requirements

OPERATING SYSTEM

Windows 7 SP1

Windows Server 2008 R2

Windows Server 2012 R2

Windows 10

Windows Server 2016

WINDOWS 7 SP1, WINDOWS SERVER 2008 R2, WINDOWS SERVER 2012 R2, WINDOWS 10, WINDOWS SERVER 2016

x64 

MEMORY SPEED

1333 MHz 

MEMORY CAPACITY

8 GB 

CPU SPEED

2.2 Gigahertz Intel Compatible

SERVER DRIVE SIZE

500 GB

SERVER DRIVE TYPE

SATA for better performance or RAID if data persistence is required.

NETWORK ADAPTER

Dual Gigabit Network Adapter

Nedladdningslänkar
X
Download Close